IMX6 SDMA ROM Script

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,859件の閲覧回数
ahmedabdelhalee
Contributor II

Dear All,

Where can I find the source code of the IMX6Q SDMA ROM script [that channel 0 executes during booting]?

I can found the source code for IMX51 on : (git://git.pengutronix.de/git/imx/sdma-firmware.git) but couldn't find the equivalent for IMX6Q.

Please reply ASAP.

Thanks in advance,

Ahmed

ラベル(1)
0 件の賞賛
返信
1 解決策
2,193件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ahmed

usually Freescale does not disclose rom sources, however

you can try entering SR ticket. Also you should provide solid reasons

why they are necessary for you.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,194件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ahmed

usually Freescale does not disclose rom sources, however

you can try entering SR ticket. Also you should provide solid reasons

why they are necessary for you.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信