IMX6 RGMII voltage tolerance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 RGMII voltage tolerance

ソリューションへジャンプ
1,570件の閲覧回数
mcggoal
Contributor I

Hi, Experts

We have a AR8031(PHY) which RGMII IO voltage(VDDIO_REG) is 1.8V, and the IMX6 use the 1.5V for the NVCC_RGMII.

AR8031 RGMII IO voltage seems could not be set to 1.5V.

My question is, could the IMX6 1.5v RGMII interface compatible with the PHY's 1.8V ?

Thanks!

0 件の賞賛
返信
1 解決策
1,564件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mcggoal

 

one can look at datasheet of used device, for example for i.MX6Q 

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

 

1.jpg1.jpg

so for PHY's 1.8V  it is necessary to use NVCC_RGMII 1.70V-1.90V

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,565件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mcggoal

 

one can look at datasheet of used device, for example for i.MX6Q 

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

 

1.jpg1.jpg

so for PHY's 1.8V  it is necessary to use NVCC_RGMII 1.70V-1.90V

 

Best regards
igor

0 件の賞賛
返信