IMX6 Platform SDK update ??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 Platform SDK update ??

3,435 次查看
marktwainjr
Contributor II

Hello Freescale,

When can we expect update over Platform SDK v1.1 for IMX6?

we are more interested in USB host driver update specifically for Mass Storage devices.

Can anyone tell me which USB Host controller chip is used on IMX6q? is it same across kinetis boards?

Thanks,

MT

标记 (5)
0 项奖励
回复
5 回复数

2,849 次查看
Yuri
NXP Employee
NXP Employee

As for i.MX6 USB - it uses ARC / Transdimension IP.

0 项奖励
回复

2,849 次查看
YixingKong
Senior Contributor IV

Yuri, could you continue the discussion with the customer?

Thanks,

Yixing

0 项奖励
回复

2,849 次查看
marktwainjr
Contributor II

Hello Yuri & All,

Thanks!!

What about USB IP in kinetis, is it same as used in IMX6?

How about using

USB Stack Product Summary Page

? Can we use this for imx6 psdk?

Q>>>>>When can we expect update over Platform SDK v1.1 for IMX6? Specifically updates for USB host driver update specifically for Mass Storage devices.

Thanks,

MT

0 项奖励
回复

2,848 次查看
YixingKong
Senior Contributor IV

Mark, please click Correct Answer/Helpful Answer if your questions have been answered.

Thanks,

Yixing

0 项奖励
回复

2,849 次查看
Yuri
NXP Employee
NXP Employee

I looked at "K20 Sub-Family Reference Manual". There are two USB modules here :

- Universal Serial Bus OTG Controller (USBOTG) ;

- USB High Speed OTG Controller (USBHS).

As I see, the USBHS is ARC IP based and it is very similar to i.MX6 OTG, at least,
so called USB-Core Registers. Note, the i.MX6 OTG also has so called non-core
(USB) registers, which are Freescale specific.
So, there is ARC USB core part of USB modules of i.MX6 and Kinetis which is practically
the same for both ones, but some specific registers also may be found.  
 

As for the USB Stack, the i.MX6 is not supported there (I think because of the mentioned specifics). 

0 项奖励
回复