IMX6 OTP Register programming with TRACE32 script via Lauterbach

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 OTP Register programming with TRACE32 script via Lauterbach

1,670 Views
blsoft
Contributor I

Hi,

I'm a beginner in the IMX6 debugging with Trace32 software.

The connection works with IMX6 processor.

I tried to read out the OTP registers with the TRACE32 sample script

but the following error message generated:

bus error at address ANSD:0x21BC010

at the Data.Set command. See below.

; first configure the timing parameters
; the following values are valid after Reset
Data.Set AD:&ocotpBase+0x10 %Long (0x5<<22.)|(6<<16.)|(0x1<<12.)|(0x299<<0.)

Could you please help me?

Thank you in advance!

 

0 Kudos
Reply
1 Reply

1,647 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the enclosed application note

0 Kudos
Reply