IMX6 NAND boot debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 NAND boot debugging

ソリューションへジャンプ
4,405件の閲覧回数
rickardandersso
Contributor IV

I am currently working with trying to boot from NAND flash on a IM6UL board. My problem is that something fails early and I do not know how far I got in the boot process. According to documentation there is  a pointer to a boot log at 0x1e0. In the boot log at 0x00901d14 I can see that there are a few entries starting with 0x10002 and ending with 0x70033.

My question is where I can find documentation describing the codes in the boot log?

ラベル(2)
0 件の賞賛
返信
1 解決策
4,206件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rickard

may be useful attached file and below link, though I am afraid boot log is not documented.

i.MX6Q NAND boot issues 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
4,206件の閲覧回数
rickardandersso
Contributor IV

Thanks, this helped! I am now successfully booting from my NAND flash.

0 件の賞賛
返信
4,206件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rickard

may be useful attached file and below link, though I am afraid boot log is not documented.

i.MX6Q NAND boot issues 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------