IMX6 JTAG (OpenOCD)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 JTAG (OpenOCD)

7,195 Views
dominicmusgrove
Contributor I

Hello,

I have a IMX6 board which I am trying to program via JTAG.

I have an XDS100V2 programmer and OpenOCD V0.10.0

OpenOCD seems to connect to the IMX6, however it errors and doesn't allow further operation.

I have successfully programmed it via the USB serial downloader and run programs/DDR3 stress test so I know the board is good.

Please see the console output below:

This is on a completely blank/un-programmed IMX6 out of reset with JTAG_MOD=0:

Open On-Chip Debugger 0.10.0
Licensed under GNU GPL v2
For bug reports, read
        http://openocd.org/doc/doxygen/bugs.html

Info : to use this adapter you MUST add ``init; ftdi_set_signal PWR_RST 1; jtag arp_init'' to the end of your config file!

Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'.
Warn : imx6.sdma: nonstandard IR value
adapter speed: 1000 kHz
Info : clock speed 1000 kHz
Info : JTAG tap: imx6.dap tap/device found: 0x4ba00477 (mfg: 0x23b (ARM Ltd.), part: 0xba00, ver: 0x4)
Info : TAP imx6.sdma does not have IDCODE
Info : JTAG tap: imx6.sjc tap/device found: 0x2191c01d (mfg: 0x00e (Freescale (Motorola)), part: 0x191c, ver: 0x2)
Info : imx6.cpu.0: hardware has 6 breakpoints, 4 watchpoints
Info : TAP imx6.dap does not have IDCODE
Info : JTAG tap: imx6.sdma tap/device found: 0x00000001 (mfg: 0x000 (<invalid>), part: 0x0000, ver: 0x0)
Info : TAP imx6.sjc does not have IDCODE
Info : TAP auto0.tap does not have IDCODE
Info : TAP auto1.tap does not have IDCODE
Info : TAP auto2.tap does not have IDCODE
Warn : AUTO auto0.tap - use "jtag newtap auto0 tap -irlen 2 -expected-id 0x00000000"
Error: auto0.tap: IR capture error; saw 0x0003 not 0x0001
Error: Invalid ACK (7) in DAP response
Polling target imx6.cpu.0 failed, trying to reexamine
Error: Invalid ACK (7) in DAP response
Error: Invalid ACK (7) in DAP response
Error: Invalid ACK (7) in DAP response

....

Error: Could not initialize the debug port
Examination failed, GDB will be halted. Polling again in 100ms

When I do a "scan_chain"

> scan_chain
   TapName             Enabled  IdCode     Expected   IrLen IrCap IrMask
-- ------------------- -------- ---------- ---------- ----- ----- ------
 0 imx6.dap               Y     0x00000000 0x4ba00477     4 0x01  0x0f
 1 imx6.sdma             Y     0x00000001 0x00000000     4 0x00  0x0f
 2 imx6.sjc                 Y     0x00000000 0x0191c01d     5 0x01  0x1f
                                           0x2191c01d
                                           0x2191e01d
                                           0x1191c01d
 3 auto0.tap              Y     0x00000000 0x00000000     2 0x01  0x03
 4 auto1.tap              Y     0x00000000 0x00000000     0 0x00  0x00
 5 auto2.tap              Y     0x00000000 0x00000000     0 0x00  0x00

I call this using:

openocd -f interface\ftdi\xds100v2.cfg -f target\imx6.cfg

Please provide any advise to get this to work.

Regards

Dominic

Labels (1)
0 Kudos
Reply
2 Replies

5,488 Views
dominicmusgrove
Contributor I

Hi Igor,

Thank you for the response, unfortunately the website is blocked at my work place, however I believe I have got it working by removing the command "jtag arp_init" from my configuration file and I am now able to read/write to internal registers.

Regards

Dominic

0 Kudos
Reply

5,488 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dominic

one can look at description on

Programming Guide: OpenOCD + Eclipse + Jtag debug on Uboot & Linux 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply