imx6ul ecspi4 w25q32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul ecspi4 w25q32

4,642件の閲覧回数
xinjianlu
Contributor II

在imx6ul下设置挂载W25Q32FV(备注支持SPI nor)

设备树配置如下:

&ecspi4 {
 fsl,spi-num-chipselects = <4>;
 cs-gpios = <&gpio2 15 0>;
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_ecspi4_1 &pinctrl_ecspi4_cs_1>;
 status = "okay";
 flash: m25p80@0 {
  compatible = "sst,w25q32","spi-nor";
  spi-max-frequency = <30000000>;
  reg = <0>;
 };

};

烧写完启动如下信息

m25p80 spi3.0: unrecognized JEDEC id bytes: 00,  0,  0

应该是 JEDEC ID 没有识别,请问设备树是否配置正确?

ecspi3下挂载的spi nor芯片的空间如何挂载 到mtd下

&ecspi4 {
 fsl,spi-num-chipselects = <4>;
 cs-gpios = <&gpio2 15 0>;
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_ecspi4_1 &pinctrl_ecspi4_cs_1>;
 status = "okay";
 flash: m25p80@0 {
  compatible = "sst,w25q32","spi-nor";
  spi-max-frequency = <30000000>;
  reg = <0>;

   partition@6 {
  label = "w25q32";
  reg = <0x20000000 0x800000>;
 };

/*

在原512Mbyte的NAND FLASH下扩8Mbyte的spi nor空间

*/
 };

};

请帮指导!!!!

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

4,203件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

for jedec spi please check documentation linux/Documentation/devicetree/bindings/mtd/jedec,spi-nor.txt

http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/Documentation/devicetree/bindings/mtd/j... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,204件の閲覧回数
xinjianlu
Contributor II

这个已看过,也参考这个,请有方面经验的人帮忙一下

0 件の賞賛
返信

4,203件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

you can debug it using sect.3.8 SPI NOR Flash Memory Technology Device (MTD)

attached Linux Manual and AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf

Best regards
igor

0 件の賞賛
返信