IMX6 HDMI PINOUT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,411件の閲覧回数
jasonl
Contributor II

Hello there,

I have the IMX6 datasheet with HDMI pinout. However, I don't know what the pins correspond to the connector. I.E, is the pins ordered from left to right or right to left on the connector facing up?

Screenshot from 2017-10-25 14-21-44.png

Thanks,

Jason 

0 件の賞賛
返信
1 解決策
2,169件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jason 

please check available documentation for that board on its vendor

NXP/Freescale i.MX 6 based ARM Computer Module - Colibri iMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,170件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jason 

please check available documentation for that board on its vendor

NXP/Freescale i.MX 6 based ARM Computer Module - Colibri iMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------