IMX6 FCB block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 FCB block

2,665 Views
rickardandersso
Contributor IV

What are the requirements on the OOB area when writing the FCB block? Can I write whatever I want in the OOB area associated with the FCB block or does it have to be empty?

Labels (1)
0 Kudos
Reply
3 Replies

2,470 Views
rickardandersso
Contributor IV

I understand, but it would be really nice to know if I am allowed to put other information in the OOB area of the FCB block? Also do I really have to write the FCB block with raw write? Or can I write it with standard ECC?

0 Kudos
Reply

2,470 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 specifics are shown in section 8.5.2.5 (Bad Block Handling in the ROM)

of i.MX6 D/Q RM.

Regards,

Yuri.

0 Kudos
Reply

2,470 Views
Yuri
NXP Employee
NXP Employee

Hello,

  It is highly recommended to use the kobs-ng utility for writing NAND FCB.

Please refer to MFG tool "NAND Flash" configuration in ucl2.xml

 

Kong-ng is part of NXP Linux BSP.

 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply