IMX6 External Interrupt trigger configuratio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 External Interrupt trigger configuratio

1,523件の閲覧回数
rajniks
Contributor I

I have few interfaces working on 2.5V and they are generating interrupts at 2.5V. Can we configure the interrupt pins to work at 2.5V level or we need to translate these 2.5V level signals to 3.3C using buffers.

ラベル(4)
0 件の賞賛
返信
1 返信

1,319件の閲覧回数
Yuri
NXP Employee
NXP Employee

  To be fully on safe side it makes sense to apply voltage buffers between 2.5 V and 3.3V
signals. But one can try to analyze carefully acceptable low and high voltage levels of the signals,
using their hardware specs : perhaps there are no problems. For example - minimal output
high voltage level of 2.5V part is greater than minimal input high level of 3.3V device.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信