IMX6 External Interrupt trigger configuratio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 External Interrupt trigger configuratio

1,524 Views
rajniks
Contributor I

I have few interfaces working on 2.5V and they are generating interrupts at 2.5V. Can we configure the interrupt pins to work at 2.5V level or we need to translate these 2.5V level signals to 3.3C using buffers.

Labels (4)
0 Kudos
Reply
1 Reply

1,320 Views
Yuri
NXP Employee
NXP Employee

  To be fully on safe side it makes sense to apply voltage buffers between 2.5 V and 3.3V
signals. But one can try to analyze carefully acceptable low and high voltage levels of the signals,
using their hardware specs : perhaps there are no problems. For example - minimal output
high voltage level of 2.5V part is greater than minimal input high level of 3.3V device.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply