IMX6 Ethernet Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Ethernet Performance

3,076 Views
ashokp
Contributor I

Hi All,

We are using IMX6 custom board and latest yocto BSP from freescale. When we testing the performance of the Ethernet we saw the performance is not good when we use the managed switches. We observed the Tx rates around 250- 400Mb/s with no errors running bi-directional test. But Rx rates around 40-90Mb/s with errors.

We didn't face this issues with unmanaged switches we are facing the issue only with manage switches. We are using managed Cisco switches 3750 and 2950.

We have gone through the freescale errata about the limitation of the Ethernet throughput.

“Limitation of ENET throughput to around 400 Mbps. ENET remains fully compatible to 1Gb standard in terms of protocol and physical signaling. If the TX and RX peak data rate is higher than 400 Mbps, there is a risk of ENET RX FIFO overrun.”

http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Please clarify what is supposed to happen with data rate goes over the error limit imposed in the errata?

Thanks,

P.Ashok

0 Kudos
Reply
1 Reply

2,103 Views
b36401
NXP Employee
NXP Employee

Please make sure that bandwidth loss is not caused with switch limitations.

As you get no issue using unmanaged switch there should be no issue with managed switch as well.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply