IMX6 EIM chip select address range partitioning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 EIM chip select address range partitioning

1,625 次查看
brianbusingye
Contributor I

Hi,

Please clarify the following.

1) I would like to partition the EIM chip selects to 32M, is this done by setting IOMUXC_GPR1[1:2] = IOMUXC_GPR1[4:5] = IOMUXC_GPR1[7:8] = IOMUXC_GPR1[10:11] = 0

2) As specified on page 1955 of IMX6DQ Applications Processor Manual, if the address range of the four chip selects is set to 32M is the range below for each chip select correct

CS0: 0x8000000 -> 0x9FFFFFF

CS1: 0xA000000 -> 0xBFFFFFF

CS2: 0xC000000 -> 0xDFFFFFF

CS3: 0xE000000 -> 0xFFFFFFF

Thanks

Brian

标签 (1)
0 项奖励
回复
1 回复

1,448 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Brian

I think your understanding is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复