IMX6 Camera driver porting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 Camera driver porting

3,234件の閲覧回数
viswanathreddy
Contributor I

Hi All,

I am the beginner of the camera drivers .

Currently i am using imx6  board , i am using the ov5640 mipi camera device.

IMX6 in Boundary device source code i browsed inside the code TWO MIPI CSI Drivers is avilable.

one is for              : drivers/media/platform/mxc/capture   

second one is for : drivers/media/platform/mxc/subdev

i am confusing which one is the correct driver .

Thanks

Viswa 

ラベル(1)
0 件の賞賛
返信
1 返信

2,328件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Viswa

subdev driver is used for new processors like i.MX6UL, 7D with PxP, CMOS Sensor Interface (CSI)

configurations. Please also refer to attached Linux Manual with drivers description.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信