IMX6 Android BSP kernel version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 Android BSP kernel version

2,110 次查看
joechiang
Contributor I

Hi sir, as we know the IMX6 newest Android BSP is JB4.3_1.1.0 and the kernel version is 3.0.35, do you have any plan/schedule to upgrade kernel to 3.8 or above version?

Thanks!

标签 (3)
0 项奖励
回复
2 回复数

1,269 次查看
VladanJovanovic
NXP Employee
NXP Employee

Hi, please check with your local sales office for detailed plans regarding kernel upgrades.

0 项奖励
回复

1,269 次查看
varsmolta
Contributor V

Any updates on this? Does Freescale intend to provide a later 3.10.x kernel with the android jb 4.3 or 4.4 releases? It seems power management is much better in the later kernels (compared to 3.0.35_4.1.0). I am getting the following errors on my custom board running jb4.3

BUG: soft lockup - CPU#1 stuck for 22s! [kinteractiveup:1358]

Modules linked in:

Pid: 1358, comm:       kinteractiveup

CPU: 1    Not tainted  (3.0.35-gde33f0b-dirty #7)

PC is at generic_exec_single+0x6c/0x90

LR is at arch_send_call_function_single_ipi+0x34/0x38

pc : [<c00bfba0>]    lr : [<c0052c4c>]    psr: 200e0013

sp : d6b6fe28  ip : 00000000  fp : c0a267d0

r10: 00000001  r9 : c14568c8  r8 : 01411000

r7 : c14568c0  r6 : 00000000  r5 : c14568c0  r4 : d6b6fe54

r3 : 00000001  r2 : f2a01000  r1 : 00000005  r0 : c0700a0c

Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c53c7d  Table: 236c404a  DAC: 00000015

0 项奖励
回复