IMX6 ALSA question sample rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 ALSA question sample rate

5,072件の閲覧回数
clement22
Contributor II

Hi,

I have a question about how linux deal with audio sample rate.

I'm using an IMX6 SABRE board with an IMX6DL. I replaced the audio codec WM8962 with an other codec.

I implemented a new codec and machine driver and playing/recording works fine.

But something is bugging me :

ALSA always set codec and platform sample rate to 48KHz, no matter what is the actual music sample rate.

For example, here is what I see when I start a music with a sample rate of 176.4KHz :

aplay -v music-wav

M: Rate conversion PCM (48000, sformat=S16_LE)
Converter: linear-interpolation
Protocol version: 10002
Its setup is:
  stream       : PLAYBACK
  access       : RW_INTERLEAVED
  format       : S16_LE
  subformat    : STD
  channels     : 2
  rate         : 176400
  exact rate   : 176400 (176400/1)
  msbits       : 16
  buffer_size  : 60211
  period_size  : 7526
  period_time  : 42666
  tstamp_mode  : NONE
  tstamp_type  : MONOTONIC
  period_step  : 1
  avail_min    : 7526
  period_event : 0
  start_threshold  : 60211
  stop_threshold   : 60211
  silence_threshold: 0
  silence_size : 0
  boundary     : 1972994048
Slave: Direct Stream Mixing PCM
Its setup is:
  stream       : PLAYBACK
  access       : MMAP_INTERLEAVED
  format       : S16_LE
  subformat    : STD
  channels     : 2
  rate         : 48000
  exact rate   : 48000 (48000/1)
  msbits       : 16
  buffer_size  : 16384
  period_size  : 2048
  period_time  : 42666
  tstamp_mode  : NONE
  tstamp_type  : MONOTONIC
  period_step  : 1
  avail_min    : 2048
  period_event : 0
  start_threshold  : 16384
  stop_threshold   : 16384
  silence_threshold: 0
  silence_size : 0
  boundary     : 1073741824
Hardware PCM card 0 'cs47l24-audio' device 0 subdevice 0
Its setup is:
  stream       : PLAYBACK
  access       : MMAP_INTERLEAVED
  format       : S16_LE
  subformat    : STD
  channels     : 2
  rate         : 48000
  exact rate   : 48000 (48000/1)
  msbits       : 16
  buffer_size  : 16384
  period_size  : 2048
  period_time  : 42666
  tstamp_mode  : ENABLE
  tstamp_type  : MONOTONIC
  period_step  : 1
  avail_min    : 2048
  period_event : 0
  start_threshold  : 1
  stop_threshold   : 1073741824
  silence_threshold: 0
  silence_size : 1073741824
  boundary     : 1073741824
  appl_ptr     : 0
  hw_ptr       : 0

So I'm wondering : why ALSA is configuring codec/platform at 48KHz and resampling the file output instead of configuring directly the codec with the good sample rate ?

In the platform/codec driver there is a structure setting the range of possible sample rate :  snd_soc_dai_driver->playback.rates

For codec it's set to : SNDRV_PCM_RATE_8000_192000

For platfrom it's set to : SNDRV_PCM_RATE_CONTINUOUS

It seems to be correctly configured, so why keeping the same sample rate ?

If anybody have an idea, thank you :smileywink:

ラベル(1)
0 件の賞賛
返信
1 返信

4,273件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Clement

please check imx6qdl.dtsi, in particular fsl,asrc-rate

linux-2.6-imx.git - Freescale i.MX Linux Tree 

linux/Documentation/devicetree/bindings/sound/fsl,asrc.txt

and Chapter 29 Asynchronous Sample Rate Converter (ASRC) Driver

attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信