IMX6 27MHz on CSI_MCLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 27MHz on CSI_MCLK

9,865 Views
umit_kayacik
Contributor II

Hi,

I am tring to take 27Mhz from IMX6 Sabresd board from GPIO_0_CLKO pin.

pastedImage_1.png

How can i do that? I guess 24Mhz is default set in DTS but i couldnt see any clock in this pin on ossiloscope? Do i need to change DTS also?

Cheers,

Umit.

7 Replies

9,479 Views
igorpadykov
NXP Employee
NXP Employee

Hi Umit

24MHz is defined in linux/arch/arm/boot/dts/imx6qdl-sabresd.dtsi :

ov564x: ov564x@3c

imx6qdl-sabresd.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

and one can test check this clock on NXP Sabre board with Demo Images from

i.MX Software | NXP 

OV564x drivers are described in sect.6.1.2 Omnivision Camera attached Linux Manual.

For obtaining 27Mhz it is necessary to modify driver or better add CCM_CCOSR initialization to uboot,

set some suitable parent clock (probably changing some PLL frequency), so 27Mhz clock

can be divided from parent clock.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

9,479 Views
umit_kayacik
Contributor II

Hi Igor,

I even download sample images for older version (L4.1.15_1.0.0-ga_images_MX6QDLSOLO) for SabreSD, i cannot still see the 24Mhz on "GPIO_0_CLKO". 

Do you want me to test spesific version of kernel that CSI_MCLK is generated correctly?

Note : prev version of kernel was yocto somo 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbe

Umit

0 Kudos
Reply

9,479 Views
igorpadykov
NXP Employee
NXP Employee

Hi Umit

what board tested, custom or i.MX6Q Sabre SD board.

MCLK configuration can be debugged in camera driver, for example in

linux/drivers/media/platform/mxc/capture/ov5640.c

ov5640.c\capture\mxc\platform\media\drivers - linux-imx - i.MX Linux kernel 

Linux configuration is described in sect.6.1.2 Omnivision Camera

attached Linux Manual.

Uboot MCLK (CKO1) configuration example:

uboot-imx/tree/board/toradex/colibri_imx6/colibri_imx6.c

colibri_imx6.c\colibri_imx6\toradex\board - uboot-imx - i.MX U-Boot 

Best regards
igor

0 Kudos
Reply

9,479 Views
umit_kayacik
Contributor II

I am using i.MX6Q Sabre SD evaluation board. I ve just download the image and create a sdcard from it. 

But i cannot see the CSI_MCLK on the above pin. Actually i dont have camera module(OV564x) so it is not connected to board.

I simply want to see 24Mhz (then i will try to see 27mhz) CSI_MCLK pin(GPIO_0_CLKO).

Umit.

0 Kudos
Reply

9,479 Views
igorpadykov
NXP Employee
NXP Employee

suggest to connect camera module and then check CSI_MCLK. 

Alternatively you can try to configure it in uboot, as in above example.

Best regards
igor

0 Kudos
Reply

9,479 Views
umit_kayacik
Contributor II

Hi Igor,

Now i can see the 27mhz clock on the pin but clock is getting down when kernel started. 

I guess one of the driver resets the CSI MCLK. This is base kernel code there is no update or any module on that. 

How can i fix this? 

Cheers

0 Kudos
Reply

9,479 Views
igorpadykov
NXP Employee
NXP Employee

Hi Umit

suggest to connect camera module and then check CSI_MCLK. 

 

Best regards
igor

0 Kudos
Reply