How to calculate Required mA= NxCxVx(0.5xF) in i.MX8MM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to calculate Required mA= NxCxVx(0.5xF) in i.MX8MM

1,124 Views
andychien
Contributor III

Dear Sir,

Our customer see schematic of i.MX8MM EVK.

See required mA= NxCxVx(0.5xF) on power table.

Could you tell us how to calculate it?

Thanks,

NxCxVx(0.5xF).bmp

Labels (1)
0 Kudos
3 Replies

1,007 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

please note that this formula is just raw estimation, for example

N=1 pin, C =30pF  (30* 10**(-12) ), U=3V, F= 100MHz (100* (10**8))

I=5mA.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,007 Views
andychien
Contributor III

Hi sir,

For your example: 

N=1 pin, C =30pF  (30* 10**(-12) ), U=3V, F= 100MHz (100* (10**8))

Imax=1x30* 10**(-12) x3x(0.5x100* (10**8))=4.5mA (not 5mA right????)

For NVCC_DRAM_1V1

N=68

C=30PF

V=1.1V

F=1.5GHz

Imax=NxCxVx(0.5xF)=68*30p*1.1*(0.5*1.5G)=1.683A

The current seem big, please help check it is right.

Thanks,

0 Kudos

1,007 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

formula is given for rough theoretical estimation.

Real life case numbers one can find in

i.MX 8M Mini Power Consumption Measurement

Best regards
igor

0 Kudos