IMX53 QSB to IMX53 QSB-R migrate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX53 QSB to IMX53 QSB-R migrate

跳至解决方案
3,888 次查看
leonidandronov2
Contributor I

Hi, I have made kernel image and root filesystem  for IMX53 QSB in past. Now I need to work with new revision of IMX53 QSB (IMX53 QSB-R). And I get some strange behavior on new boards with kernel from old ones. Some usb devices are not recognize... Nothing is working realy...

What I need to do? I use Ubuntu vmware image with ltib 9.1 on it. Do I need to change some configs for kernel build?

标签 (1)
0 项奖励
回复
1 解答
3,707 次查看
fabio_estevam
NXP Employee
NXP Employee

I have seen this same issue. In order to solve it you need to upgrade your bootloader.

U-boot should detect the board type and pass this information to the kernel via ATAGs.

You can use U-boot mainline or the latest one from git.freescale.com (11.09 branch). Both of these versions detects the board type correctly, pass this info to the kernel and then the kernel will configure USB correctly.

在原帖中查看解决方案

0 项奖励
回复
7 回复数
3,708 次查看
fabio_estevam
NXP Employee
NXP Employee

I have seen this same issue. In order to solve it you need to upgrade your bootloader.

U-boot should detect the board type and pass this information to the kernel via ATAGs.

You can use U-boot mainline or the latest one from git.freescale.com (11.09 branch). Both of these versions detects the board type correctly, pass this info to the kernel and then the kernel will configure USB correctly.

0 项奖励
回复
3,707 次查看
leonidandronov2
Contributor I

Thank you!

I have solved this by downloading a new vmware Ubuntu image and compiling system newly. With new uboot and kernel everything works.

0 项奖励
回复
3,707 次查看
aksispd
Contributor II

This might be the right place to ask: I'm running the VM ubuntu that came on the CD with the i.MX53 QSB-R board and when I'm running ltib does not see the options I expect (device driver), when running make menuconfig I got these items but seems the architecture is not passed on and a bunch of options are not shown (nothign specific to the i.MX processor, e.g. MXC/capture). Can you tell me which version of VM ubuntu you used that seemed to work with the QSB-R? Did you use ltib config interface?

Thanks

0 项奖励
回复
3,707 次查看
Yuri
NXP Employee
NXP Employee

Hello,


  You may try the VMware Linux image with development tools and i.MX53 Linux 11.09

BSP installed and configured for the MCIMX53-START-R and the MCIMX53-START :

https://www.freescale.com/webapp/Download?colCode=IMX53_QSB_UBUNTU_VM&appType=license&location=null

Regards,

Yuri.

0 项奖励
回复
3,707 次查看
aksispd
Contributor II

Yuri,

that is what I'm using and after installing ltib in the config interface there is nothing that configures device drivers, everything else seems to be correct. If I understand correctly the QSB the START and the LOCO board are the same. What am I missing?

0 项奖励
回复
3,707 次查看
Yuri
NXP Employee
NXP Employee

Hi,

Yes - for MX53 START board, select your board  as mx53_loco.

Please use "i.MX53_START_Linux_BSP_UserGuide.pdf" in BSP documentation

for more  details.

Regards,

Yuri.

0 项奖励
回复
3,707 次查看
aksispd
Contributor II

Thanks, got it. Had to realized it's under kernel config

0 项奖励
回复