IMX53 QSB cannot start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53 QSB cannot start

2,806 Views
marshallzhou
Contributor I

Hi guys,

         I am a totally newbie with QSB, when I plugin the power, the FLT and 5V led light on. While I plugin the UART with my computer, seems computer cannot distinguish any new port. At the same time, when I press poweron button, the LCD has no display. Anything wrong with the board? Months before, it can start correctly. What happen? How can I diagnose? Thanks.

Labels (1)
0 Kudos
Reply
6 Replies

2,693 Views
Yuri
NXP Employee
NXP Employee

Please check power voltages of i.MX53. Sometimes, because of "bad" power adapter, providing glitches, the PMIC may be damaged.   

2,693 Views
marshallzhou
Contributor I

Thanks for ur reply, I'v used the original power adapter, I think it's ok.  I doubt if it's the os issue or the board is broken.  While I cannot get log from serial port, I totally don't know how to begin. Is there any way I can be sure the board is ok?  Any way to access the "BIOS" like PC or something like that?

0 Kudos
Reply

2,693 Views
Yuri
NXP Employee
NXP Employee

> ... I'v used the original power adapter ...

Good adapter - is "heavy" adapter.

After pressing power on practically all leds (except FLT) should shine.
If not - problems with power.

0 Kudos
Reply

2,693 Views
marshallzhou
Contributor I

Hi Yuri Muhin, After pressing power on, only the FLT and 5v led of the QSB shine, just as when plugin the power. And u said "If not - problems with power.", I thought that means the adapter is broken, after I bought the new one, the problem is same. And I can hear the board make a sound "zizi sisi" all the time. Any idea? How can I find the problem? Really thanks.

0 Kudos
Reply

2,694 Views
Yuri
NXP Employee
NXP Employee

Please check power supply voltages of i.MX53 chip - I am afraid PMIC of the QSB does not provide the voltages at all.

0 Kudos
Reply

2,694 Views
marshallzhou
Contributor I

Oops, I am not sure. Where is the chip, and how can I check it? I don't know the hardware at all. I am reaally confused with the integrated board.:smileyconfused:

0 Kudos
Reply