IMX53 Application Development

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53 Application Development

1,627 Views
MichaelGale
Contributor II

Hi - I'm trying to set up a build environment for creating applications on the QuickStart and/or the SABRE tablet. The goal is to build an OpenGL Gnome application; I would like to use the VMWare Ubuntu image which shipped with both products as my host environment. Is there a particular way IMX53 developers are creating a build environment for applications?

Is "ltib" the normal way applications are developed for this platform? I could install a cross-compiler on my host, but I don't want to manage and build all of the dependencies if I can avoid it.

I see that the pre-built Ubuntu image contains the OpenGL ES v2 library as well as the SDL, and PNG libraries, so I'm hoping there is a way to recreate that environment.

 

Thanks,

Michael

Tags (1)
0 Kudos
Reply
1 Reply

1,510 Views
MichaelGale
Contributor II

I'm going to assume something like this is the preferred process, unless there is a better way...

http://imxcommunity.org/group/imxqt/forum/topics/building-qt-for-imx5x

0 Kudos
Reply