IMX515 Fuze Bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,234件の閲覧回数
wysockilukasz
Contributor II

Hello,

I have problem with IIC module for IM515. I'm traing to burn fuse bits using Lauterbach Jtag and

programing sequency from RM (page 1174).
For example for fuse FB0REG1 ADDR: 0x83f98844 (default value:0x00)

I would like to achieve value 0x60 (set BT_LPB_FREQ[2:0] = b011)

To do that I'm wrote a short script in TRACE32:

//////////////////////first bit

//Write 8’hAA to PRG_P

     Data.Set d:83F98028 %l 0xAA

//User writes target bit address to UPA/LPA using IP Bus

//UA

     Data.Set d:83F98014 %l 0x00

//LA

     Data.Set d:83F98018 %l 0x8D

//User sets PRG bit

     Data.Set d:83F98010 %l 0x01

//Set PROGD in STAT

     Data.Set d:83F98000 %l 0x02

///////////////////////// second bit

//Write 8’hAA to PRG_P

     Data.Set d:83F98028 %l 0xAA

//User writes target bit address to UPA/LPA using IP Bus

//UA

     Data.Set d:83F98014 %l 0x00

//LA

     Data.Set d:83F98018 %l 0x8E

//User sets PRG bit

     Data.Set d:83F98010 %l 0x01

//Set PROGD in STAT

     Data.Set d:83F98000 %l 0x02

////////////////////////third bit is 0!

After I will execute it  FB0REG1 = 0x60 but when I reset the cpu FUSE back to the default value = 00.

It is not important how the imx boot moode (Internal Boot / Internal Boot-ROM Selected)

Mayby I don't understand algorytm.

Can anyone can help my?

Lukas.

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
2,116件の閲覧回数
wysockilukasz
Contributor II

Problem solved!

The algorithm above is correct but I also need to set the bit:

efuse_prog_supply_gate (CGPR -> 0x73FD_4064),

(and additional information, you must have a 3.3 V on pin VDD_FUSE).


Lukas.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,117件の閲覧回数
wysockilukasz
Contributor II

Problem solved!

The algorithm above is correct but I also need to set the bit:

efuse_prog_supply_gate (CGPR -> 0x73FD_4064),

(and additional information, you must have a 3.3 V on pin VDD_FUSE).


Lukas.

0 件の賞賛
返信