IMX512 Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX512 Flash

4,263件の閲覧回数
ajayachandran
Contributor I

Hi ,

I am trying to flash my MCIMX512CJM6C in advanced toolkit through usb port in mode HAB

But i am getting an error "No usb detected"

I have made usb type a connection as below

  • USB Pin 1- USB_OTG_VBUS
  • USB Pin 2-USB_OTG_D_N
  • USB Pin 3-USB_OTG_D_P
  • USB Pin 4-GND

but IMX512 is detecting in my pc in device manager it listing as SE Blank Elvis

is there any driver needs to be installed to detect imx512?

Please help me out to detect my imx512 to flash

Regards,

Arun

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

3,955件の閲覧回数
ajayachandran
Contributor I

i could make it work with windows XP but its doesnot work with windows 7

0 件の賞賛
返信

3,955件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Arunprasath

one can check usb recommendations in Chapter 22 Porting USB Host1 and USB OTG
https://www.nxp.com/docs/en/user-guide/MX53UG.pdf

Try with i.MX53 QSB board or with mfg tool on

i.MX537 Processors|HD Video|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,955件の閲覧回数
ajayachandran
Contributor I

Hi Igor,

I have access to only 

  • USB_OTG_VBUS
  • USB_OTG_D_N
  • USB_OTG_D_P
  • USB_OTG_ID
  • GND

Regards,

Arun

0 件の賞賛
返信

3,955件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Arunprasath

it should work with that configuration. Also one can connect through usb hub.

Best regards
igor

0 件の賞賛
返信

3,955件の閲覧回数
ajayachandran
Contributor I

Hi Igor,

  • USB Pin 1- USB_OTG_VBUS
  • USB Pin 2-USB_OTG_D_N
  • USB Pin 3-USB_OTG_D_P
  • USB Pin 4-GND

the above connection is enough? in that case why in device manager it listing as SE Blank Elvis

  • USB_OTG_ID require any connection ?

Regards,

Arun

0 件の賞賛
返信

3,955件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Arunprasath

 

USB_OTG_ID does not require any connection.

 

Best regards
igor

0 件の賞賛
返信

3,955件の閲覧回数
ajayachandran
Contributor I

Hi Igor,

then why in device manager it listing as SE Blank Elvis?

Do i need to install any driver?

Regards,

Arun

0 件の賞賛
返信

3,955件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Arunprasath

"SE Blank Elvis" is message provided by ROM,

in general you can ignore it. No need to install additional drivers.

Best regards
igor

0 件の賞賛
返信