IMX280 on Nucleus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX280 on Nucleus

1,437 次查看
rameshnair
Contributor I

Running a Nucleus kernel on an imx280 board.

When 5v input  is removed, Power STS bit 15 is still high meaning that there is power. ANy idea why?

标签 (1)
0 项奖励
回复
1 回复

1,273 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ramesh

probably voltage still high than VBUSVALID_TRSH level

(defined in register HW_POWER_5VCTRL) due to capacitor.on 5v input.

One try to ground it.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复