IMX280 on Nucleus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX280 on Nucleus

1,505 Views
rameshnair
Contributor I

Running a Nucleus kernel on an imx280 board.

When 5v input  is removed, Power STS bit 15 is still high meaning that there is power. ANy idea why?

Labels (1)
0 Kudos
Reply
1 Reply

1,341 Views
igorpadykov
NXP Employee
NXP Employee

Hi ramesh

probably voltage still high than VBUSVALID_TRSH level

(defined in register HW_POWER_5VCTRL) due to capacitor.on 5v input.

One try to ground it.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply