IMX280 on Nucleus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX280 on Nucleus

1,470件の閲覧回数
rameshnair
Contributor I

Running a Nucleus kernel on an imx280 board.

When 5v input  is removed, Power STS bit 15 is still high meaning that there is power. ANy idea why?

ラベル(1)
0 件の賞賛
返信
1 返信

1,306件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ramesh

probably voltage still high than VBUSVALID_TRSH level

(defined in register HW_POWER_5VCTRL) due to capacitor.on 5v input.

One try to ground it.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信