IMX28 : use DCP engine to encrypt data using AES ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX28 : use DCP engine to encrypt data using AES ?

1,743 次查看
g__
Contributor II

I installed the DCP driver into buildroot.

Is it possible to use the DCP engine of the IMX28 to encrypt data ?

If yes, do you have  a code example ?

Thanks

Best

标签 (1)
0 项奖励
回复
1 回复

1,733 次查看
igorpadykov
NXP Employee
NXP Employee

Hi g__

 

one can look at below dcp example:

https://source.codeaurora.org/external/imx/imx-optee-os/tree/core/drivers/imx/dcp/dcp.c?h=imx_5.4.47...

also one can consider cryptodev-linux/test:

https://github.com/cryptodev-linux/cryptodev-linux

Some customers tested on i.MX6ULL board, which has the same DCP module.

In Kernel Configuration, you need exclude below option (default <Y>):

Cryptographic API ---> Disable run-time self tests

The result is shown below when insert the tcrypt.ko module:

# insmod tcrypt.ko mode=10

insmod: ERROR: could not insert module tcrypt.ko: Resource temporarily unavailable

# cat /proc/interrupts

...

236:         72       GPC  46 Level     dcp-vmi-irq
237:          2       GPC  47 Level     dcp-irq

 

Best regards
igor

0 项奖励
回复