IMX28 Brownout Detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX28 Brownout Detection

Jump to solution
1,675 Views
franzforstmayr
Contributor I

Hey All,

is there any way to recognise an brownout condition by hardware?

PSWITCH stays high for a long time and RESET follows the level of VDDIO.

Yours

Franz

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,564 Views
igorpadykov
NXP Employee
NXP Employee

Hi Franz

there is no signal for brownout detection, in general

one can attach jtag debugger and read brownout comparator

condition in register HW_POWER_STS.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,565 Views
igorpadykov
NXP Employee
NXP Employee

Hi Franz

there is no signal for brownout detection, in general

one can attach jtag debugger and read brownout comparator

condition in register HW_POWER_STS.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply