IMX233 or IMX288 will support universal host controller interface (UHCI) or open host controller interface (OHCI)....?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX233 or IMX288 will support universal host controller interface (UHCI) or open host controller interface (OHCI)....?

ソリューションへジャンプ
2,018件の閲覧回数
kishorepoojari
Contributor III

Hello All,

Wether IMX233 or IMX285 will support universal host controller interface (UHCI) or open host controller interface (OHCI) .....?

Regards,

Kishore P

ラベル(1)
0 件の賞賛
返信
1 解決策
1,760件の閲覧回数
art
NXP Employee
NXP Employee

None of the processors you've specified support UHCI/OHCI interfaces. Both processors have integrated USB PHY modules.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,761件の閲覧回数
art
NXP Employee
NXP Employee

None of the processors you've specified support UHCI/OHCI interfaces. Both processors have integrated USB PHY modules.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信