IMX233 or IMX288 will support universal host controller interface (UHCI) or open host controller interface (OHCI)....?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX233 or IMX288 will support universal host controller interface (UHCI) or open host controller interface (OHCI)....?

Jump to solution
1,989 Views
kishorepoojari
Contributor III

Hello All,

Wether IMX233 or IMX285 will support universal host controller interface (UHCI) or open host controller interface (OHCI) .....?

Regards,

Kishore P

Labels (1)
0 Kudos
Reply
1 Solution
1,731 Views
art
NXP Employee
NXP Employee

None of the processors you've specified support UHCI/OHCI interfaces. Both processors have integrated USB PHY modules.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,732 Views
art
NXP Employee
NXP Employee

None of the processors you've specified support UHCI/OHCI interfaces. Both processors have integrated USB PHY modules.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply