IMX233 256MB SLC NAND ecc problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX233 256MB SLC NAND ecc problem

1,078件の閲覧回数
xubovey
Contributor III

Hi all

I have a problem when i use NAND FLASH with IMX233, when i try use "md5sum -c" to check my rootfs in nand, i get some failed, howerver i cannot read nand ecc error corrected log.

a. i have try crypress-S34ML02G100TF100,  sumsung-K9F2G08U0A, they get the same question.

b. i have known the mtd rst bug, and i have checked the driver has fixed the bug.

c. my kernel version was 2.6.35

d. i try boot from sd and then try "nandtest -k /dev/mtd1" command and sucessed.

e. command "cat /sys/devices/platform/gpmi-nfc.0/mtd_info" get the same status as follow log:

Name : gpmi-nfc-main
Type : 4
Flags : 0x00000400
Size in Bytes : 268435456
Erase Region Count : 0
Erase Size in Bytes: 131072
Write Size in Bytes: 2048
OOB Size in Bytes : 64
Errors Corrected : 0
Failed Reads : 0
Bad Block Count : 9
BBT Block Count : 0
ECC Byte Count : 0
OOB Available Bytes: 64
[ 0, 64]

I cannot get ecc corrected log  in all my boards, but some boards(about 30%) md5sum was success with no failed. 

Please help me to solve the problem?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)