IMX23 Unencrypted Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX23 Unencrypted Boot

2,102件の閲覧回数
paolomartinetti
Contributor I

Hi everybody,

I would like to write the key in IMX233 OTP registers, and support unencrypted boot.

I have used BitBurner to blow ENABLE_UNENCRYPTED_BOOT and to write the four key registers.

After update (which installs UNENCRYPTED linux image and expands UNENCRYPTED root file system) the system is unable to boot,

emitting error '0x80501006' error (Key dictionary lookup failed).

What does it mean?

Any suggestion?

Thanks in Advance

Paolo

ラベル(1)
0 件の賞賛
返信
1 返信

1,790件の閲覧回数
Yuri
NXP Employee
NXP Employee

"  In default build, the '-z' option is passed to the elftosb utility and a default zero key is

added to the boot image. It is because the default zero key does not match with the
CRYPTO_KEY OTP fuses on your device, this firmware will not boot.

  After ENABLE_UNENCRYPTED_BOOT fuse is blown, the ROM expects an image either is encrypted
with a correct crypto key or not encrypted by any key. Thus both encrypted/unencrypted images are

valid to boot when this fuse is blown.

  To generate an unencrypted image, please remove the "-z" option [...] of elftosb."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信