IMX1176 RGB TFT LCD Example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX1176 RGB TFT LCD Example

跳至解决方案
405 次查看
tbayram
Contributor IV

Hello Everybody,

 

Im working on IMX1176 & Custom LCD TFT LCD (not mipi). İs there any example about this subject? 

Thanks for all

0 项奖励
回复
1 解答
385 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @tbayram,

I recommend you to refer to our GUI Guider/lvgl example codes, as they are well suited for the RK055HDMIPI4MA0 and RK043FN02H-CT TFT LDC displays that we ship with our i.MX RT devices. You could do so either using GUI Guider as described on this community post: https://community.nxp.com/t5/GUI-Guider/To-dumb-on-a-TFT-disply/td-p/1714007

Or directly from the SDK on MCUXpresso by importing an example from the "lvgl_examples" subfolder:

EdwinHz_0-1703028184301.png

I would highly recommend using GUI Guider as it is great and user friendly tool for using display technologies with our i.MX RT family.

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
1 回复
386 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @tbayram,

I recommend you to refer to our GUI Guider/lvgl example codes, as they are well suited for the RK055HDMIPI4MA0 and RK043FN02H-CT TFT LDC displays that we ship with our i.MX RT devices. You could do so either using GUI Guider as described on this community post: https://community.nxp.com/t5/GUI-Guider/To-dumb-on-a-TFT-disply/td-p/1714007

Or directly from the SDK on MCUXpresso by importing an example from the "lvgl_examples" subfolder:

EdwinHz_0-1703028184301.png

I would highly recommend using GUI Guider as it is great and user friendly tool for using display technologies with our i.MX RT family.

BR,
Edwin.

0 项奖励
回复