IMX processor for PSTN Telephony feature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX processor for PSTN Telephony feature

4,981件の閲覧回数
guslabao
Contributor III

Hi, I am looking for an IMX processor that can support PSTN telephony feature such as DTMF generation, AEC,LEC,CID.  The processor is cable of running Android.  Does anyone have any recommedation?  Thanks.

8 返答(返信)

4,712件の閲覧回数
abhijeet_ghodga
Contributor III

Hi guslabao‌,

Rather than the reference design, do you have any drivers to support the 8-bit Mu Law data received from the PSTN phones?

I have already tried fsl-ssi driver and ALSA driver and they do not capture data, but they are able to send data to phone.

Best,

Abhijeet

0 件の賞賛
返信

4,712件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Gus,

I'm not familiar with PSTN Telephony but you would be using a chip that would connect to the board by, lets say, I2C right?, can you give me more info?

0 件の賞賛
返信

4,712件の閲覧回数
guslabao
Contributor III

Hi Sergio,

PSTN is the telephone line.  I want to design a phone that will connect to the telephone line by adding a DAA circuit for the Analog Front End. 

The DAA circuit will connect to the host processor that can do telephony features such as DTMF generation, AEC,LEC,CID.


See the Freescale DSP56858 device which supports telephone features. 

I am looking for an host processor that have integrated DSP to support the telephone feature set.  The host processor need to be powerful enough to run Android.  The DSP will already have the software telephony feature support, as well.


Hope this clarifies things.


Thanks,

Gus

4,712件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Gus,

All of the i.MX6 processors have a NEON co-processor:

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0409e/index.html

I did some research and I know of customers that have used the i.MX6s and i.MX6Q for PSTN

0 件の賞賛
返信

4,712件の閲覧回数
guslabao
Contributor III

HI Sergio,

I did notice that IMX6 have been used on PSTN phones.  I wanted to find out if Freescale have a reference design with the IMX6s that is used in PSTN designs.

I was hoping to have the software telephony features available as a package as well. 

Thanks.

4,712件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Gus,

Unfortunately we do not have a reference design for the i.MX and PSTN phones.

Please let me know of any question you may have.

0 件の賞賛
返信

4,712件の閲覧回数
sumit8915
Contributor III

HI Gus,

   You can use a SLIC IC and DAA IC that can support the telephony features such as DTMF generation, AEC,LEC,CID and can be interfaced to the host processor through standard interfaces. But i am not pretty much sure what kind of SW implementation you will need to do on the i.MX6 processor.

thanks

4,712件の閲覧回数
guslabao
Contributor III

Thanks Sumit.  I was looking more for a processor that have the telephony feature software part of the package.

0 件の賞賛
返信