IMX PCIe port link down

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX PCIe port link down

6,751件の閲覧回数
xiaoqiangyang
Contributor III

Hi all,

I am testing iwl4965 on mini pcie port of MX6Q SABRESD. After linux boot, I can see noting using 'lspci',and I find these messages during boot up:

...

...

iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

PCIE: imx_pcie_pltfm_probe start link up.

link up failed, DB_R0:0x002f0200, DB_R1:0x08200000!

IMX PCIe port: link down!

IMX usb wakeup probe

...

My BSP is L3.0.35_4.1.0_130816 downloaded from freescale,and I add support of pcie in kernel:

System Type --->Freescale MXC Implementations --->[*] PCI Express support

Bus support ---> PCI Express support

Device Drivers ---> Network device support --->Wireless LAN ---> <*> Intel Wireless WiFi 4965AGN (iwl4965)

Adding EC and RC support have no help.

Anyone knows the reason? Are there some places I need pay attention to?

Thanks in advance!

Xiaoqiang

0 件の賞賛
返信
9 返答(返信)

5,384件の閲覧回数
minshi
Contributor I

Can you tell me, how do you solve this problem?

0 件の賞賛
返信

5,384件の閲覧回数
wallyyeh
Contributor V

I don't even know how to call you, sir. Your name become just a bunch of utf8 codes I guess.

first, this question is not solved since the author never change this question's status.

but if you just want to know "how to reset PCIE device", here's the simple description:

every pcie device must have an reset pin, and most HW design will attach a GPIO on it, what you need is just toggle the GPIO.

hope this will be help.

0 件の賞賛
返信

5,384件の閲覧回数
minshi
Contributor I

Thank you very much

     But I'm a beginner, i still want to ask:

     link up failed,DB....

     what should I do ?

     The JTAG1 is the reset pin?If this is the case,Our development board did not lead to the pin.

     But my colleague has link up sucess,use the same hardware.But he had other problems.

0 件の賞賛
返信

5,384件の閲覧回数
wallyyeh
Contributor V

Hi, 明时:

    I just copy the name from mail, sorry. :smileygrin:

    You mention you're using development board, so could you also provide some information about your pcie device, board model and SDK version? for example, I use freescale's development borad - "SabreSD", and using SDK3.0.35_4.1.0

    You also mention your coworker using same code, same device but didn't met this issue. Did you two change the device and see if you got a broken board/pcie device?

   In kernel/arch/arm/mach-mx6/pcie.c, "link up failed" error occur while imx_pcie_link_up() execute, you can take a look.

Wally

0 件の賞賛
返信

5,384件の閲覧回数
minshi
Contributor I

Hi,Wally:

     First,very thanks for you.

     Then,I use the development borad which modelled on the freescale's development borad - "SabreSD", and using SDK3.0.35_4.1.0.

     We only have one development board,mycoworker is debugged a year ago.

     I also read that code, but I didn't find any problem.

how can I do?

明时

0 件の賞賛
返信

5,384件の閲覧回数
wallyyeh
Contributor V

Dear 明时:

   OK, if you using sabreSD, the PCIE reset pin is GPIO17(which is group 7, pin 12).

At kernel/arch/arm/mach-mx6/board-mx6q_sabresd.c, you will find the pcie reset pin's define:

#define SABRESD_PCIE_RST_B_REVBIMX_GPIO_NR(7, 12)

Since I'm not pcie expert, my only suggestion is toggle this GPIO while u-boot, and if this trick doesn't work, you may need open a tech support request from NXP.

Wally

0 件の賞賛
返信

5,384件の閲覧回数
minshi
Contributor I

Dear Wally:

     Can you give me a schematic diagram?

     In schematic diagram,i can not find the GPIO17.

Best wishes。

明时

0 件の賞賛
返信

5,384件の閲覧回数
wallyyeh
Contributor V

Dear 明时:

    Sorry, I don't have it either.I usually get informed by asking our HW mates or Freescale FAE.

If you can't find it on the NXP website, just ask the FAE for it.

Wally

0 件の賞賛
返信

5,384件の閲覧回数
wallyyeh
Contributor V

just a suggestion, do you reset your pcie device before you start your kernel?

I do reset in arch/arm/mach-mx6/board-mx6q_sabresd.c

0 件の賞賛
返信