About pin assign in i.MX6 SoloX.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About pin assign in i.MX6 SoloX.

Jump to solution
1,495 Views
keitanagashima
Senior Contributor I


Dear All,

Device : i.MX6 SoloX (MCIMX6X1CVO08AB)

First, refer to "Table 118. 17x17 mm NP (no PCIe) supplies contact assignments" in IMX6SXIEC(Rev.1).

L9 pin was defined as VDD_SOC_CAP.

Next, refer to attached file.

L9 pin was defined as VDD_SOC_IN* in OrCAD symbol.

Which is right?

Best Regards,

Keita

Labels (1)
0 Kudos
Reply
1 Solution
1,247 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

it should be VDD_SOC_IN for "L9" pin

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,247 Views
keitanagashima
Senior Contributor I

Dear Igor,

Hello. Thank you for you reply.

> it should be VDD_SOC_IN for "L9" pin

Let me confirm again.

Refer to "Table 127. i.MX 6SoloX Data Sheet Document Revision History" in IMX6SXIEC(Rev.1).

There is below description.

-----

In Table 118, "17x17 mm NP (no PCIe) supplies contact assignments," on page 164, added ball L9 to the VDD_SOC_CAP row

-----

Is the description typo?

If the data sheet's description was typo, could you request about modification the document?

Best Regards,

Keita

0 Kudos
Reply
1,247 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

this DS typo will be corrected, as mentioned in application team answer on

https://community.freescale.com/message/628537

you can access to that thread with help of local fae.

Best regards

igor

0 Kudos
Reply
1,247 Views
keitanagashima
Senior Contributor I

Dear Igor,

Thank you for your quick response!

OK. Thank you very much.

Best Regards,

Keita

0 Kudos
Reply
1,248 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

it should be VDD_SOC_IN for "L9" pin

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply