IMX IMAGE FLASH to sdcard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX IMAGE FLASH to sdcard

Jump to solution
2,674 Views
athul_am
Contributor II

hi,

I am trying to take an image into the sdcard,

i tried using the uuu command.

sudo uuu -b sd_all u-boot-imx6ull14x14evk.imx fsl-image-qt6-imx6ull14x14evk.wic.zst


uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Wait for Known USB Device Appear...

it is getting stuck here.

Please help on how to proceed

0 Kudos
Reply
1 Solution
2,636 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Yes, that is correct.

Please make sure to select the serial download boot mode changing the switches.

Best regards.

View solution in original post

0 Kudos
Reply
4 Replies
2,637 Views
athul_am
Contributor II

hi @JorgeCas ,

so to flash i should mount the sdcard on the board and then connect the serial connector and then run the command .

Is my understanding correct,if not please let me know 

Thanks in advance

0 Kudos
Reply
2,637 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Yes, that is correct.

Please make sure to select the serial download boot mode changing the switches.

Best regards.

0 Kudos
Reply
2,658 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It seems that your board is not in serial download mode.

Please confirm it using next command:

uuu -lsusb

JorgeCas_0-1710448073770.png

Best regards.

0 Kudos
Reply
2,610 Views
athul_am
Contributor II

hi @JorgeCas ,

Thanks for the reply, i will check this.

0 Kudos
Reply