IMX IMAGE FLASH to sdcard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX IMAGE FLASH to sdcard

ソリューションへジャンプ
2,631件の閲覧回数
athul_am
Contributor II

hi,

I am trying to take an image into the sdcard,

i tried using the uuu command.

sudo uuu -b sd_all u-boot-imx6ull14x14evk.imx fsl-image-qt6-imx6ull14x14evk.wic.zst


uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Wait for Known USB Device Appear...

it is getting stuck here.

Please help on how to proceed

0 件の賞賛
返信
1 解決策
2,593件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Yes, that is correct.

Please make sure to select the serial download boot mode changing the switches.

Best regards.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,594件の閲覧回数
athul_am
Contributor II

hi @JorgeCas ,

so to flash i should mount the sdcard on the board and then connect the serial connector and then run the command .

Is my understanding correct,if not please let me know 

Thanks in advance

0 件の賞賛
返信
2,594件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Yes, that is correct.

Please make sure to select the serial download boot mode changing the switches.

Best regards.

0 件の賞賛
返信
2,615件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It seems that your board is not in serial download mode.

Please confirm it using next command:

uuu -lsusb

JorgeCas_0-1710448073770.png

Best regards.

0 件の賞賛
返信
2,567件の閲覧回数
athul_am
Contributor II

hi @JorgeCas ,

Thanks for the reply, i will check this.

0 件の賞賛
返信