IMX 93 boot image container set ELE FW padding.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 93 boot image container set ELE FW padding.

852 Views
logan3c3
Contributor III

Hello, While referring to AHAB secure boot document i found out that for imx93 3 containers are being used. one for ELE (Nxp container) another of SPL img and CM33 ,last one for ATF, U-boot.

Its said that a padding is applied for ELE (I hope its for the rom code to understand where the image is). But there is a confusion in the secure boot layout

Anzal3c3_0-1735985559522.png

here ele fw is represented after 2nd container set header and signature. The first container only has padding which is not true as the document says 1st container is for ELE FW

 

Can anyone help with this what is the possible explanation for this??

IMX93QSB 

Labels (1)
0 Kudos
Reply
1 Reply

824 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

The first container for ELE firmware is correct. As the layout is based on the offset for each image.

Harvey021_1-1736328131413.png

Can also refer to the RM about container header

 

Regards

Harvey

0 Kudos
Reply