IMX 93 GUI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 93 GUI

2,212 Views
Mohan51
Contributor II

Hi, I am using IMX93-EVK and implemented a sample live image capturing program using opencv .with the help of IMX-MIPI-HDMI, I connected to Monitor. while powering the board the monitor display "Wayland Terminal". and i the terminal i executed the sample program.but getting errors. I am posting my simple program and the error i am facing.

I am using the Latest Linux image:Linux 6.6.3_1.0.0

Program:

 

import cv2

# Create a VideoCapture object
cap = cv2.VideoCapture(0)

# Check if the camera opened successfully
if not cap.isOpened():
print("Error: Could not open camera.")
exit()

# Loop to continuously capture frames from the camera
while True:
# Capture frame-by-frame
ret, frame = cap.read()

# Check if frame is successfully captured
if not ret:
print("Error: Failed to capture frame.")
break

# Display the captured frame
cv2.imshow('Live Camera', frame)

# Check for the 'q' key press to exit the loop
if cv2.waitKey(1) & 0xFF == ord('q'
break

# Release the VideoCapture object and close all OpenCV windows
cap.release()
cv2.destroyAllWindows()

 

 

Error:

 

Traceback (most recent call last):
File "/home/root/ml-object-detection-examples-for-imx93-main/detectnet_v2/simple.py", line 22, in <module>
cv2.imshow('Live Camera', frame)
cv2.error: OpenCV(4.9.0) /io/opencv/modules/highgui/src/window.cpp:1272: error: (-2:Unspecified error) The function is not implemented. Rebuild the library with Windows, GTK+ 2.x or Cocoa support. If you are on Ubuntu or Debian, install libgtk2.0-dev and pkg-config, then re-run cmake or configure script in function 'cvShowImage'

 

 

Note: How to access GUI in imx93 board,and how to display the images.

 

0 Kudos
Reply
3 Replies

2,173 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, you might try the xwayland Distro. This error is present when you have a bad image or it has no installed completely OpenCV.

Regards

 

0 Kudos
Reply

2,168 Views
Mohan51
Contributor II

@Bio_TICFSL I wrote a simple opencv program when but giving error while executing cv2.imshow() and cv2.destroyAllWindows() methods only...

 

 

Where I need to find xwayland distro..is it like the latest BSP(i.e Linux6.6.3)

0 Kudos
Reply

2,161 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Compile and Install the full-image on your board to get the opencv without errors.

Regards

0 Kudos
Reply