IMX 8m Mini EVK wifi (WLAN) not showing after boot from Linux image on SDCard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 8m Mini EVK wifi (WLAN) not showing after boot from Linux image on SDCard

Jump to solution
26,430 Views
imranhassan
Contributor II

I am trying to boot IMX 8M Mini LPDDR4 EVK. I loaded image from the NXP website (LF_v6.6.23-2.0.0_images_IMX8MMEVK). After boot I checked wifi by command ifconfig I got NO wlan.

What could be issue not to having wlan to connect wifi.

The output of ifconfig is as follow
 

root@imx8mmevk:~# ifconfig
eth0: flags=-28669<UP,BROADCAST,MULTICAST,DYNAMIC> mtu 1500
ether 00:04:9f:08:97:37 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0

lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 91 bytes 7727 (7.5 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 91 bytes 7727 (7.5 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0

 

 

The output of boot is as follow


U-Boot SPL 2024.04+g674440bc73e+p0 (Jun 06 2024 - 10:05:34 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0:  RNG instantiated
Normal Boot
Trying to boot from MMC1
NOTICE:  Do not release JR0 to NS as it can be used by HAB
NOTICE:  BL31: v2.10.0  (release):android-14.0.0_2.0.0-rc1-1-g49143a170
NOTICE:  BL31: Built : 10:04:22, May 29 2024


U-Boot 2024.04+g674440bc73e+p0 (Jun 06 2024 - 10:05:34 +0000)

CPU:   i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 46C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM:  2 GiB
TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
Core:  220 devices, 35 uclasses, devicetree: separate
MMC:   FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22

        [0] lcdif@32e00000, video
        [1] mipi_dsi@32e10000, video_bridge
        [2] adv7535@3d, panel
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22
In:    serial
Out:   serial
Err:   serial
SEC0:  RNG instantiated
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net:   eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0
Working FDT set to 43000000
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
starting USB...
Bus usb@32e40000: Port not available.
USB is stopped. Please issue 'usb start' first.
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
48263 bytes read in 5 ms (9.2 MiB/s)
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
switch to partitions #0, OK
mmc2(part 0) is current device
Scanning mmc 2:1...
47924 bytes read in 14 ms (3.3 MiB/s)
Error: Cannot initialize UEFI sub-system, r = 3
Running BSP bootcmd ...
switch to partitions #0, OK
mmc1 is current device
Failed to load 'boot.scr'
35355136 bytes read in 598 ms (56.4 MiB/s)
Booting from mmc ...
48263 bytes read in 4 ms (11.5 MiB/s)
## Flattened Device Tree blob at 43000000
   Booting using the fdt blob at 0x43000000
Working FDT set to 43000000
   Using Device Tree in place at 0000000043000000, end 000000004300ec86
Working FDT set to 43000000
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.6.23-lts-next-06236-gb586a521770e (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.2.0, GNU ld (GNU Binutils) 2.42.0.20240216) #1 SMP PREEMPT Fri Jun  7 13:15:57 UTC 2024
[    0.000000] KASLR enabled
[    0.000000] Machine model: FSL i.MX8MM EVK board
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000096000000, size 640 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x0000000096000000..0x00000000bdffffff (655360 KiB) map reusable linux,cma
[    0.000000] OF: reserved mem: 0x00000000be000000..0x00000000bfdfffff (30720 KiB) nomap non-reusable optee_core@be000000
[    0.000000] OF: reserved mem: 0x00000000bfe00000..0x00000000bfffffff (2048 KiB) nomap non-reusable optee_shm@bfe00000
[    0.000000] NUMA: No NUMA configuration found
[    0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bdffffff]
[    0.000000] NUMA: NODE_DATA [mem 0x95bce6c0-0x95bd0fff]
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000040000000-0x00000000bdffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000040000000-0x00000000bdffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bdffffff]
[    0.000000] On node 0, zone DMA: 8192 pages in unavailable ranges
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.4
[    0.000000] percpu: Embedded 22 pages/cpu s50536 r8192 d31384 u90112
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: kernel page table isolation forced ON by KASLR
[    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk1p2 rootwait rw
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Fallback order for Node 0: 0
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 508032
[    0.000000] Policy zone: DMA
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 4.
[    0.000000] software IO TLB: mapped [mem 0x000000008f800000-0x0000000093800000] (64MB)
[    0.000000] Memory: 1266988K/2064384K available (20992K kernel code, 1630K rwdata, 7756K rodata, 3968K init, 643K bss, 142036K reserved, 655360K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 128 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[    0.000000] ITS: No ITS available, not enabling LPIs
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[    0.000001] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[    0.000442] Console: colour dummy device 80x25
[    0.000506] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[    0.000517] pid_max: default: 32768 minimum: 301
[    0.000585] LSM: initializing lsm=capability,integrity
[    0.000674] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.000686] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.002219] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[    0.002300] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[    0.002469] rcu: Hierarchical SRCU implementation.
[    0.002473] rcu:     Max phase no-delay instances is 1000.
[    0.003659] EFI services will not be available.
[    0.003871] smp: Bringing up secondary CPUs ...
[    0.004414] Detected VIPT I-cache on CPU1
[    0.004482] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[    0.004524] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.005069] Detected VIPT I-cache on CPU2
[    0.005116] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[    0.005140] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.005610] Detected VIPT I-cache on CPU3
[    0.005653] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[    0.005675] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.005746] smp: Brought up 1 node, 4 CPUs
[    0.005752] SMP: Total of 4 processors activated.
[    0.005756] CPU features: detected: 32-bit EL0 Support
[    0.005759] CPU features: detected: 32-bit EL1 Support
[    0.005763] CPU features: detected: CRC32 instructions
[    0.005826] CPU: All CPU(s) started at EL2
[    0.005848] alternatives: applying system-wide alternatives
[    0.007703] devtmpfs: initialized
[    0.014982] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.015006] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.033615] pinctrl core: initialized pinctrl subsystem
[    0.035721] DMI not present or invalid.
[    0.036350] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.037377] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[    0.037496] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.037611] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.037681] audit: initializing netlink subsys (disabled)
[    0.037803] audit: type=2000 audit(0.036:1): state=initialized audit_enabled=0 res=1
[    0.038327] thermal_sys: Registered thermal governor 'step_wise'
[    0.038331] thermal_sys: Registered thermal governor 'power_allocator'
[    0.038366] cpuidle: using governor menu
[    0.038569] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.038655] ASID allocator initialised with 32768 entries
[    0.039578] Serial: AMBA PL011 UART driver
[    0.039648] imx mu driver is registered.
[    0.039668] imx rpmsg driver is registered.
[    0.046274] platform soc@0: Fixed dependency cycle(s) with /soc@0/bus@30000000/efuse@30350000/unique-id@4
[    0.049866] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[    0.050553] platform 30350000.efuse: Fixed dependency cycle(s) with /soc@0/bus@30000000/clock-controller@30380000
[    0.051707] platform 30350000.efuse: Fixed dependency cycle(s) with /soc@0/bus@30000000/clock-controller@30380000
[    0.058201] platform 32e00000.lcdif: Fixed dependency cycle(s) with /soc@0/bus@32c00000/mipi_dsi@32e10000
[    0.058428] platform 32e00000.lcdif: Fixed dependency cycle(s) with /soc@0/bus@32c00000/mipi_dsi@32e10000
[    0.058537] platform 32e10000.mipi_dsi: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a30000/adv7535@3d
[    0.058566] platform 32e10000.mipi_dsi: Fixed dependency cycle(s) with /soc@0/bus@32c00000/lcdif@32e00000
[    0.058836] platform 32e20000.csi1_bridge: Fixed dependency cycle(s) with /soc@0/bus@32c00000/mipi_csi@32e30000
[    0.059069] platform 32e20000.csi1_bridge: Fixed dependency cycle(s) with /soc@0/bus@32c00000/mipi_csi@32e30000
[    0.059186] platform 32e30000.mipi_csi: Fixed dependency cycle(s) with /soc@0/bus@32c00000/csi1_bridge@32e20000
[    0.059262] platform 32e30000.mipi_csi: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a40000/ov5640_mipi@3c
[    0.059912] platform 32e40000.usb: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a30000/tcpc@50
[    0.065532] Modules: 2G module region forced by RANDOMIZE_MODULE_REGION_FULL
[    0.065559] Modules: 0 pages in range for non-PLT usage
[    0.065563] Modules: 515488 pages in range for PLT usage
[    0.066247] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.066253] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.066258] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.066263] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.066267] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.066272] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.066276] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.066281] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.068214] ACPI: Interpreter disabled.
[    0.069174] iommu: Default domain type: Translated
[    0.069183] iommu: DMA domain TLB invalidation policy: strict mode
[    0.069500] SCSI subsystem initialized
[    0.069812] usbcore: registered new interface driver usbfs
[    0.069840] usbcore: registered new interface driver hub
[    0.069868] usbcore: registered new device driver usb
[    0.070979] mc: Linux media interface: v0.10
[    0.071015] videodev: Linux video capture interface: v2.00
[    0.071079] pps_core: LinuxPPS API ver. 1 registered
[    0.071083] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.071094] PTP clock support registered
[    0.071263] EDAC MC: Ver: 3.0.0
[    0.071683] scmi_core: SCMI protocol bus registered
[    0.072082] FPGA manager framework
[    0.072164] Advanced Linux Sound Architecture Driver Initialized.
[    0.072861] Bluetooth: Core ver 2.22
[    0.072903] NET: Registered PF_BLUETOOTH protocol family
[    0.072907] Bluetooth: HCI device and connection manager initialized
[    0.072915] Bluetooth: HCI socket layer initialized
[    0.072920] Bluetooth: L2CAP socket layer initialized
[    0.072931] Bluetooth: SCO socket layer initialized
[    0.073279] vgaarb: loaded
[    0.073798] clocksource: Switched to clocksource arch_sys_counter
[    0.073998] VFS: Disk quotas dquot_6.6.0
[    0.074026] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.074186] pnp: PnP ACPI: disabled
[    0.081012] NET: Registered PF_INET protocol family
[    0.081158] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.082708] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[    0.082737] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.082750] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.082898] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[    0.083363] TCP: Hash tables configured (established 16384 bind 16384)
[    0.083457] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.083503] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.083659] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.084083] RPC: Registered named UNIX socket transport module.
[    0.084088] RPC: Registered udp transport module.
[    0.084090] RPC: Registered tcp transport module.
[    0.084093] RPC: Registered tcp-with-tls transport module.
[    0.084095] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.085136] PCI: CLS 0 bytes, default 64
[    0.085496] kvm [1]: IPA Size Limit: 40 bits
[    0.087524] kvm [1]: GICv3: no GICV resource entry
[    0.087530] kvm [1]: disabling GICv2 emulation
[    0.087545] kvm [1]: GIC system register CPU interface enabled
[    0.087570] kvm [1]: vgic interrupt IRQ9
[    0.087590] kvm [1]: Hyp mode initialized successfully
[    0.088771] Initialise system trusted keyrings
[    0.088945] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[    0.089216] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.089428] NFS: Registering the id_resolver key type
[    0.089449] Key type id_resolver registered
[    0.089452] Key type id_legacy registered
[    0.089470] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.089476] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.089493] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    0.089674] 9p: Installing v9fs 9p2000 file system support
[    0.122152] Key type asymmetric registered
[    0.122157] Asymmetric key parser 'x509' registered
[    0.122197] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[    0.122203] io scheduler mq-deadline registered
[    0.122207] io scheduler kyber registered
[    0.122232] io scheduler bfq registered
[    0.129175] EINJ: ACPI disabled.
[    0.139685] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[    0.139702] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[    0.145563] mxs-dma 33000000.dma-controller: initialized
[    0.147012] SoC: i.MX8MM revision 1.0
[    0.147470] Bus freq driver module loaded
[    0.160101] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.163128] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 18, base_baud = 5000000) is a IMX
[    0.163256] serial serial0: tty port ttymxc0 registered
[    0.163777] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 19, base_baud = 5000000) is a IMX
[    0.164450] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 20, base_baud = 1500000) is a IMX
[    0.164476] printk: console [ttymxc1] enabled
[    1.462628] imx-drm display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[    1.470378] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[    1.477409] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e10000 to encoder DSI-34: -517
[    1.489089] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[    1.497363] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -517
[    1.511597] loop: module loaded
[    1.516436] megasas: 07.725.01.00-rc1
[    1.525517] spi-nor spi0.0: n25q256ax1 (32768 Kbytes)
[    1.534880] tun: Universal TUN/TAP device driver, 1.6
[    1.540902] thunder_xcv, ver 1.0
[    1.544175] thunder_bgx, ver 1.0
[    1.547438] nicpf, ver 1.0
[    1.552405] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[    1.559642] hns3: Copyright (c) 2017 Huawei Corporation.
[    1.564994] hclge is initializing
[    1.568355] e1000: Intel(R) PRO/1000 Network Driver
[    1.573241] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    1.579018] e1000e: Intel(R) PRO/1000 Network Driver
[    1.583989] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    1.589947] igb: Intel(R) Gigabit Ethernet Network Driver
[    1.595394] igb: Copyright (c) 2007-2014 Intel Corporation.
[    1.601004] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    1.607282] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    1.613380] sky2: driver version 1.30
[    1.617626] usbcore: registered new device driver r8152-cfgselector
[    1.623928] usbcore: registered new interface driver r8152
[    1.629876] VFIO - User Level meta-driver version: 0.3
[    1.637962] usbcore: registered new interface driver uas
[    1.643318] usbcore: registered new interface driver usb-storage
[    1.649394] usbcore: registered new interface driver usbserial_generic
[    1.655950] usbserial: USB Serial support registered for generic
[    1.661983] usbcore: registered new interface driver ftdi_sio
[    1.667756] usbserial: USB Serial support registered for FTDI USB Serial Device
[    1.675100] usbcore: registered new interface driver usb_serial_simple
[    1.681652] usbserial: USB Serial support registered for carelink
[    1.687773] usbserial: USB Serial support registered for flashloader
[    1.694152] usbserial: USB Serial support registered for funsoft
[    1.700181] usbserial: USB Serial support registered for google
[    1.706133] usbserial: USB Serial support registered for hp4x
[    1.711906] usbserial: USB Serial support registered for kaufmann
[    1.718028] usbserial: USB Serial support registered for libtransistor
[    1.724583] usbserial: USB Serial support registered for moto_modem
[    1.730874] usbserial: USB Serial support registered for motorola_tetra
[    1.737514] usbserial: USB Serial support registered for nokia
[    1.743373] usbserial: USB Serial support registered for novatel_gps
[    1.749753] usbserial: USB Serial support registered for siemens_mpi
[    1.756136] usbserial: USB Serial support registered for suunto
[    1.762088] usbserial: USB Serial support registered for vivopay
[    1.768123] usbserial: USB Serial support registered for zio
[    1.773822] usbcore: registered new interface driver usb_ehset_test
[    1.783384] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[    1.798114] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[    1.804339] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 2024-02-27T17:43:43 UTC (1709055823)
[    1.814333] i2c_dev: i2c /dev entries driver
[    1.820536] mx6s-csi 32e20000.csi1_bridge: initialising
[    1.826750] mxc_mipi-csi 32e30000.mipi_csi: supply mipi-phy not found, using dummy regulator
[    1.835506] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered
[    1.842485] CSI: Registered sensor subdevice: mxc_mipi-csi.0
[    1.848173] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 333000000
[    1.862291] Bluetooth: HCI UART driver ver 2.3
[    1.866767] Bluetooth: HCI UART protocol H4 registered
[    1.871914] Bluetooth: HCI UART protocol BCSP registered
[    1.877261] Bluetooth: HCI UART protocol LL registered
[    1.882407] Bluetooth: HCI UART protocol ATH3K registered
[    1.887837] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    1.894214] Bluetooth: HCI UART protocol Broadcom registered
[    1.899908] Bluetooth: HCI UART protocol QCA registered
[    1.906794] sdhci: Secure Digital Host Controller Interface driver
[    1.912992] sdhci: Copyright(c) Pierre Ossman
[    1.917982] Synopsys Designware Multimedia Card Interface Driver
[    1.924722] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.932866] ledtrig-cpu: registered to indicate activity on CPUs
[    1.940457] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    1.947373] usbcore: registered new interface driver usbhid
[    1.952961] usbhid: USB HID core driver
[    1.962472] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[    1.970101] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    1.981267]  cs_system_cfg: CoreSight Configuration manager initialised
[    1.989034] platform soc@0: Fixed dependency cycle(s) with /soc@0/bus@30000000/efuse@30350000
[    1.998765] optee: probing for conduit method.
[    2.003249] optee: revision 4.2 (c6be5b57)
[    2.004818] optee: dynamic shared memory is enabled
[    2.014173] optee: initialized driver
[    2.020428] hantrodec 0 : module inserted. Major = 509
[    2.026196] hantrodec 1 : module inserted. Major = 509
[    2.032300] hx280enc: module inserted. Major <508>
[    2.042808] NET: Registered PF_LLC protocol family
[    2.047722] u32 classifier
[    2.050484]     input device check on
[    2.051735] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[    2.054154]     Actions configured
[    2.054798] NET: Registered PF_INET6 protocol family
[    2.061380] mmcblk2: mmc2:0001 DG4032 29.1 GiB
[    2.065358] Segment Routing with IPv6
[    2.071768]  mmcblk2: p1 p2
[    2.073439] In-situ OAM (IOAM) with IPv6
[    2.078562] mmcblk2boot0: mmc2:0001 DG4032 4.00 MiB
[    2.079913] NET: Registered PF_PACKET protocol family
[    2.085402] mmcblk2boot1: mmc2:0001 DG4032 4.00 MiB
[    2.088694] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    2.095606] mmcblk2rpmb: mmc2:0001 DG4032 4.00 MiB, chardev (234:0)
[    2.099403] Bluetooth: RFCOMM TTY layer initialized
[    2.122751] Bluetooth: RFCOMM socket layer initialized
[    2.127904] Bluetooth: RFCOMM ver 1.11
[    2.131668] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    2.136986] Bluetooth: BNEP filters: protocol multicast
[    2.142224] Bluetooth: BNEP socket layer initialized
[    2.147198] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    2.153126] Bluetooth: HIDP socket layer initialized
[    2.158829] 8021q: 802.1Q VLAN Support v1.8
[    2.163047] lib80211: common routines for IEEE802.11 drivers
[    2.168762] 9pnet: Installing 9P2000 support
[    2.173204] Key type dns_resolver registered
[    2.178277] NET: Registered PF_VSOCK protocol family
[    2.204517] registered taskstats version 1
[    2.208762] Loading compiled-in X.509 certificates
[    2.235720] gpio gpiochip0: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    2.246301] gpio gpiochip1: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    2.256856] gpio gpiochip2: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    2.267408] gpio gpiochip3: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    2.277989] gpio gpiochip4: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    2.291356] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests
[    2.299603] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests
[    2.308055] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests
[    2.316257] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests
[    2.325960] i2c i2c-0: IMX I2C adapter registered
[    2.331986] adv7511 1-003d: supply avdd not found, using dummy regulator
[    2.338819] adv7511 1-003d: supply dvdd not found, using dummy regulator
[    2.341208] nxp-pca9450 0-0025: pca9450a probed.
[    2.345590] adv7511 1-003d: supply pvdd not found, using dummy regulator
[    2.356924] adv7511 1-003d: supply a2vdd not found, using dummy regulator
[    2.363755] adv7511 1-003d: supply v3p3 not found, using dummy regulator
[    2.370497] adv7511 1-003d: supply v1p2 not found, using dummy regulator
[    2.378346] adv7511 1-003d: Probe failed. Remote port 'mipi_dsi@32e10000' disabled
[    2.386155] platform 32e40000.usb: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a30000/tcpc@50
[    2.395949] i2c 1-0050: Fixed dependency cycle(s) with /soc@0/bus@32c00000/usb@32e40000
[    2.408675] i2c i2c-1: IMX I2C adapter registered
[    2.419231] pca953x 2-0020: using no AI
[    2.431487] ov5640_mipi 2-003c: No sensor reset pin available
[    2.437308] ov5640_mipi 2-003c: supply DOVDD not found, using dummy regulator
[    2.444580] ov5640_mipi 2-003c: supply DVDD not found, using dummy regulator
[    2.451676] ov5640_mipi 2-003c: supply AVDD not found, using dummy regulator
[    2.471051] ov5640_mipi 2-003c: Read reg error: reg=300a
[    2.476381] ov5640_mipi 2-003c: Camera is not found
[    2.481536] i2c i2c-2: IMX I2C adapter registered
[    2.489433] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[    2.492273] imx-drm display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[    2.496786] imx6q-pcie 33800000.pcie:       IO 0x001ff80000..0x001ff8ffff -> 0x0000000000
[    2.504460] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[    2.512483] imx6q-pcie 33800000.pcie:      MEM 0x0018000000..0x001fefffff -> 0x0018000000
[    2.527680] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e10000 to encoder DSI-34: -19
[    2.539280] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[    2.547560] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -19
[    2.555232] imx-drm display-subsystem: bound 32e10000.mipi_dsi (ops imx_sec_dsim_ops)
[    2.563997] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[    2.571857] imx-drm display-subsystem: [drm] Cannot find any crtc or sizes
[    2.582794] pps pps0: new PPS source ptp0
[    2.698251] mdio_bus 30be0000.ethernet-1:00: Fixed dependency cycle(s) with /soc@0/bus@30800000/ethernet@30be0000/mdio/ethernet-phy@0/vddio-regulator
[    2.730298] imx6q-pcie 33800000.pcie: iATU: unroll T, 4 ob, 4 ib, align 64K, limit 4G
[    2.799666] fec 30be0000.ethernet eth0: registered PHC device 0
[    2.812701] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1
[    2.826685] galcore: clk_get vg clock failed, disable vg!
[    2.826862] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[    2.832671] Galcore version 6.4.11.p2.745085
[    2.857422] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[    2.871400] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[    2.886755] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 1
[    2.901341] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[    2.910083] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[    2.918805] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[    2.936641] mmc0: new ultra high speed SDR104 SDIO card at address 0001
[    2.942848] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    2.952867] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    2.959145] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[    2.966430] clk: Disabling unused clocks
[    2.970415] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    2.976059] ALSA device list:
[    2.979042] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[    2.982046]   No soundcards found.
[    3.554679] mmc1: host does not support reading read-only switch, assuming write-enable
[    3.585284] mmc1: new ultra high speed SDR104 SDXC card at address 59b4
[    3.592890] mmcblk1: mmc1:59b4       118 GiB
[    3.598936]  mmcblk1: p1 p2
[    3.722317] imx6q-pcie 33800000.pcie: Phy link never came up
[    4.731451] imx6q-pcie 33800000.pcie: Phy link never came up
[    4.737458] imx6q-pcie 33800000.pcie: PCI host bridge to bus 0000:00
[    4.743909] pci_bus 0000:00: root bus resource [bus 00-ff]
[    4.749424] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[    4.755630] pci_bus 0000:00: root bus resource [mem 0x18000000-0x1fefffff]
[    4.762554] pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400
[    4.768913] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]
[    4.775205] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref]
[    4.782038] pci 0000:00:00.0: supports D1
[    4.786068] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold
[    4.794201] pci 0000:00:00.0: BAR 0: assigned [mem 0x18000000-0x180fffff]
[    4.801008] pci 0000:00:00.0: BAR 6: assigned [mem 0x18100000-0x1810ffff pref]
[    4.808252] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[    4.813910] pcieport 0000:00:00.0: PME: Signaling with IRQ 221
[    5.990876] EXT4-fs (mmcblk1p2): recovery complete
[    6.012321] EXT4-fs (mmcblk1p2): mounted filesystem eff003a1-0ece-4ce4-b9fc-a830febd501b r/w with ordered data mode. Quota mode: none.
[    6.024524] VFS: Mounted root (ext4 filesystem) on device 179:98.
[    6.032790] devtmpfs: mounted
[    6.036670] Freeing unused kernel memory: 3968K
[    6.041544] Run /sbin/init as init process
[    6.392325] systemd[1]: systemd 255.4^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified)
[    6.424223] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 6.6-scarthgap (scarthgap)!

[    6.452135] systemd[1]: Hostname set to <imx8mmevk>.
[    6.965035] systemd[1]: Queued start job for default target Graphical Interface.
[    6.999997] systemd[1]: Created slice Slice /system/getty.
[  OK  ] Created slice Slice /system/getty.
[    7.024223] systemd[1]: Created slice Slice /system/modprobe.
[  OK  ] Created slice Slice /system/modprobe.
[    7.048209] systemd[1]: Created slice Slice /system/serial-getty.
[  OK  ] Created slice Slice /system/serial-getty.
[    7.071674] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    7.094257] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password Requests to Console Directory Watch.
[    7.118204] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password Requests to Wall Directory Watch.
[    7.142111] systemd[1]: Reached target Host and Network Name Lookups.
[  OK  ] Reached target Host and Network Name Lookups.
[    7.166251] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Path Units.
[    7.185984] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    7.209984] systemd[1]: Reached target Slice Units.
[  OK  ] Reached target Slice Units.
[    7.229986] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[    7.283916] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    7.310070] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    7.330522] systemd[1]: Listening on Syslog Socket.
[  OK  ] Listening on Syslog Socket.
[    7.350335] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    7.375878] systemd[1]: Listening on Journal Audit Socket.
[  OK  ] Listening on Journal Audit Socket.
[    7.398501] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    7.422740] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    7.443037] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    7.467516] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    7.490770] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    7.514916] systemd[1]: Listening on User Database Manager Socket.
[  OK  ] Listening on User Database Manager Socket.
[    7.562056] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    7.585460] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    7.609166] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    7.630470] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[    7.648779] systemd[1]: Mounting Temporary Directory /tmp...
         Mounting Temporary Directory /tmp...
[    7.670744] systemd[1]: Starting Create List of Static Device Nodes...
         Starting Create List of Static Device Nodes...
[    7.718976] systemd[1]: Starting Load Kernel Module configfs...
         Starting Load Kernel Module configfs...
[    7.742112] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
[    7.790920] systemd[1]: Starting Load Kernel Module fuse...
         Starting Load Kernel Module fuse...
[    7.810125] fuse: init (API version 7.39)
[    7.816610] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    7.838121] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[    7.857505] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    7.899002] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    7.921528] systemd[1]: Starting Generate network units from Kernel command line...
         Starting Generate network units from Kernel command line...
[    7.949939] systemd[1]: Starting Remount Root and Kernel File Systems...
         Starting Remount Root and Kernel File Systems systemd-journald[151]: Collecting audit messages is enabled.
[0m...
[    7.982135] systemd[1]: Starting Coldplug All udev Devices...
         Starting Coldplug All udev Devices...
[    8.010944] systemd[1]: Starting Virtual Console Setup...
         Starting Virtual Console Setup...
[    8.035129] systemd[1]: Started RPC Bind.
[    8.042774] EXT4-fs (mmcblk1p2): re-mounted eff003a1-0ece-4ce4-b9fc-a830febd501b r/w. Quota mode: none.
[  OK  ] Started RPC Bind.
[    8.067808] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory /tmp.
[  OK  ] Finished Create List of Static Device Nodes.
[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[  OK  ] Finished Load Kernel Modules.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Remount Root and Kernel File Systems.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
         Starting Apply Kernel Variables...
         Starting Create Static Device Nodes in /dev gracefully...
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Mounted Kernel Configur[    8.187854] systemd-journald[151]: Received client request to flush runtime journal.
ation File System.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Virtual Console Setup.
[  OK  ] Finished Apply Kernel Variables.
[  OK  ] Finished Create Static Device Nodes in /dev gracefully.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /var/volatile...
[    8.423973] audit: type=1334 audit(1709055830.116:2): prog-id=6 op=LOAD
[    8.430860] audit: type=1334 audit(1709055830.124:3): prog-id=7 op=LOAD
         Starting Rule-based Manager for Device Events and Files...
[  OK  ] Mounted /var/volatile.
         Starting Load/Save OS Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Finished Create Volatile Files and Directories.
[    8.608197] audit: type=1334 audit(1709055830.300:4): prog-id=8 op=LOAD
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[    8.669609] audit: type=1334 audit(1709055830.360:5): prog-id=9 op=LOAD
[    8.677095] audit: type=1334 audit(1709055830.360:6): prog-id=10 op=LOAD
         Starting User D[    8.685709] audit: type=1334 audit(1709055830.360:7): prog-id=11 op=LOAD
atabase Manager...
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[  OK  ] Started User Database Manager.
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Started Rule-based Manager for Device Events and Files.
         Starting Start Psplash Boot Screen...
[  OK  ] Started Start Psplash Boot Screen.
[  OK  ] Started Start psplash-systemd progress communication helper.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Started Daily rotation of log files.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting Docker Socket for the API...
         Starting sshd.socket...
         Starting Weston socket...
[  OK  ] Listening on Docker Socket for the API.
[  OK  ] Listening on sshd.socket.
[  OK  ] Listening on Weston socket.
[  OK  ] Reached target Socket Units.
[  OK  ] Reached target Basic System.
[  OK  ] Started Job spooling tools.
[  OK  ] Started Periodic Command Scheduler.
         Starting D-Bus System Message Bus...
[  OK  ] Started Linux Firmware Loader Daemon.
[  OK  ] Started Configuration for i.MX GPU (Former rc_gpu.S).
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 P[    9.703805] imx-sdma 30bd0000.dma-controller: firmware found.
[    9.703805] imx-sdma 302b0000.dma-controller: firmware found.

[    9.703981] imx-sdma 30bd0000.dma-controller: loaded firmware 4.6
[    9.726563] imx-sdma 302c0000.dma-controller: firmware found.
         Starting Telephony service...
[  OK  ] Started Parsec Service.
[  OK  ] Started Updates psplash to basic.
[  OK  ] Started System Logging Service.
[    9.800500] audit: type=1334 audit(1709055831.492:8): prog-id=12 op=LOAD
[    9.809226] audit: type=1334 audit(1709055831.500:9): prog-id=13 op=LOAD
[    9.818737] audit: type=1334 audit(1709055831.512:10): prog-id=14 op=LOAD
         Starting User Login Management...
         Starting OpenSSH Key Generation...
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[  OK  ] Reached target Preparation for Network.
         Starting Network Configuration...
[  OK  ] Started User Login Management.
[  OK  ] Started Network Configuration.
[  OK  ] Reached target Hardware activated USB gadget.
[  OK  ] Finished OpenSSH Key Generation.
[  OK  ] Finished Load/Save OS Random Seed.
[  OK  ] Created slice Slice /system/systemd-fsck.
[  OK  ] Created slice Slice /system/tee-supplicant.
         Starting File System Check on /dev/mmcblk2p2...
[  OK  ] Started TEE Supplicant on teepriv0.
[  OK  ] Stopped Virtual Console Setup.
         Stopping Virtual Console Setup...
         Starting Virtual Console Setup...
         Expecting device /dev/mmcblk2p1...
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Found device /dev/mmcblk2p1.
[  OK  ] Started Telephony service.
         Expecting device /dev/mmcblk1p1...
         Starting Connection service...
         Starting File System Check on /dev/mmcblk2p1...
[  OK  ] Finished Virtual Console Setup.
[  OK  ] Found device /dev/mmcblk1p1.
         Starting Save/Restore Sound Card State...
         Starting File System Check on /dev/mmcblk1p1...
[  OK  ] Finished File System Check on /dev/mmcblk2p1.
         Mounting /run/media/boot-mmcblk2p1...
[  OK  ] Finished Save/Restore Sound Card State.
[  OK  ] Reached target Sound Card.
[  OK  ] Started Connection service.
[  OK  ] Reached target Network.
         Starting Avahi mDNS/DNS-SD Stack...
         Starting containerd container runtime...
[  OK  ] Started Network Time Service.
[  OK  ] Started Update psplash to network.
         Starting Terminate Psplash Boot Screen...
         Starting Permit User Sessions...
[  OK  ] Mounted /run/media/boot-mmcblk2p1.
[FAILED] Failed to start Terminate Psplash Boot Screen.
See 'systemctl status psplash-quit.service' for details.
[  OK  ] Finished Permit User Sessions.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttymxc1.
[  OK  ] Reached target Login Prompts.
         Starting Weston, a Wayland compositor, as a system service...
         Starting WPA supplicant...
         Starting Hostname Service...
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Finished File System Check on /dev/mmcblk1p1.
         Mounting /run/media/boot-mmcblk1p1...
[  OK  ] Started Hostname Service.
[  OK  ] Started WPA supplicant.
[  OK  ] Mounted /run/media/boot-mmcblk1p1.
[  OK  ] Finished File System Check on /dev/mmcblk2p2.
         Mounting /run/media/root-mmcblk2p2...
[  OK  ] Mounted /run/media/root-mmcblk2p2.
[  OK  ] Created slice User Slice of UID 0.
         Starting User Runtime Directory /run/user/0...
[  OK  ] Finished User Runtime Directory /run/user/0.
         Starting User Manager for UID 0...
[  OK  ] Started User Manager for UID 0.
[  OK  ] Started Session c1 of User root.
[  OK  ] Started containerd container runtime.
[  OK  ] Reached target Multi-User System.
[FAILED] Failed to start Weston, a Wayland compositor, as a system service.
See 'systemctl status weston.service' for details.
[  OK  ] Reached target Graphical Interface.
         Starting Record Runlevel Change in UTMP...
[  OK  ] Finished Record Runlevel Change in UTMP.

NXP i.MX Release Distro 6.6-scarthgap imx8mmevk ttymxc1

imx8mmevk login: root

 

0 Kudos
Reply
1 Solution
26,235 Views
imranhassan
Contributor II

I figured it out. It is in the guide "i.MX Linux Users Guide LF6.1.36_2.1.0" page 109/123 (PDF attached)


# For all the Wi-Fi modules:
modprobe moal mod_para=nxp/wifi_mod_para.conf
$connmanctl
connmanctl> enable wifi
connmanctl> scan wifi
connmanctl> services /* This should list of the network. For example
 imiM                 wifi_eafb1cb95e57_696d694d_managed_psk*/
connmanctl> agent on
connmanctl> connect wifi_eafb1cb95e57_696d694d_managed_psk /* Enter Passphrase
 */
Agent RequestInput wifi_c0e4347f5053_4a62726f_managed_psk
Passphrase = [ Type=psk, Requirement=mandatory ]
Passphrase?123456
connmanctl> quit

 

ifconfig shows now

wfd0: flags=-28605<UP,BROADCAST,RUNNING,MULTICAST,DYNAMIC>  mtu 1500
        inet 192.168.45.111  netmask 255.255.255.0  broadcast 192.168.45.255
        inet6 fe80::e8fb:1cff:feb9:5e57  prefixlen 64  scopeid 0x20<link>
        ether ea:fb:1c:b9:5e:57  txqueuelen 1000  (Ethernet)
        RX packets 14  bytes 1544 (1.5 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 47  bytes 6601 (6.4 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

 

root@imx8mmevk:~# ping www.google.com
PING www.google.com (142.251.32.68) 56(84) bytes of data.
64 bytes from yyz12s07-in-f4.1e100.net (142.251.32.68): icmp_seq=1 ttl=106 time=402 ms
64 bytes from yyz12s07-in-f4.1e100.net (142.251.32.68): icmp_seq=2 ttl=106 time=219 ms
64 bytes from yyz12s07-in-f4.1e100.net (142.251.32.68): icmp_seq=3 ttl=106 time=243 ms

 

View solution in original post

0 Kudos
Reply
2 Replies
26,236 Views
imranhassan
Contributor II

I figured it out. It is in the guide "i.MX Linux Users Guide LF6.1.36_2.1.0" page 109/123 (PDF attached)


# For all the Wi-Fi modules:
modprobe moal mod_para=nxp/wifi_mod_para.conf
$connmanctl
connmanctl> enable wifi
connmanctl> scan wifi
connmanctl> services /* This should list of the network. For example
 imiM                 wifi_eafb1cb95e57_696d694d_managed_psk*/
connmanctl> agent on
connmanctl> connect wifi_eafb1cb95e57_696d694d_managed_psk /* Enter Passphrase
 */
Agent RequestInput wifi_c0e4347f5053_4a62726f_managed_psk
Passphrase = [ Type=psk, Requirement=mandatory ]
Passphrase?123456
connmanctl> quit

 

ifconfig shows now

wfd0: flags=-28605<UP,BROADCAST,RUNNING,MULTICAST,DYNAMIC>  mtu 1500
        inet 192.168.45.111  netmask 255.255.255.0  broadcast 192.168.45.255
        inet6 fe80::e8fb:1cff:feb9:5e57  prefixlen 64  scopeid 0x20<link>
        ether ea:fb:1c:b9:5e:57  txqueuelen 1000  (Ethernet)
        RX packets 14  bytes 1544 (1.5 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 47  bytes 6601 (6.4 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

 

root@imx8mmevk:~# ping www.google.com
PING www.google.com (142.251.32.68) 56(84) bytes of data.
64 bytes from yyz12s07-in-f4.1e100.net (142.251.32.68): icmp_seq=1 ttl=106 time=402 ms
64 bytes from yyz12s07-in-f4.1e100.net (142.251.32.68): icmp_seq=2 ttl=106 time=219 ms
64 bytes from yyz12s07-in-f4.1e100.net (142.251.32.68): icmp_seq=3 ttl=106 time=243 ms

 

0 Kudos
Reply
26,251 Views
imranhassan
Contributor II

Does anyone have any idea why its not working? 

 

Any kind of help will be appreciated. Thanks

0 Kudos
Reply