IMX.35 LTIB error for adding gtk+

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX.35 LTIB error for adding gtk+

1,150件の閲覧回数
Hitex
Contributor I

I am trying to include GTK+ in ltib.however it is giving error and showing dependency on cairo package.

I am unable to include cairo package as shown in the snapshot.

 

please reply at hitesh_sharma@mahindrasatyam.com

 

 

 

677-01129640036245_Cairo.png

 

checking for sigsetjmp... yes
checking for locale.h... (cached) yes
checking for LC_MESSAGES... (cached) yes
checking for libintl.h... (cached) yes
checking for ngettext in libc... (cached) yes
checking for dgettext in libc... (cached) yes
checking for bind_textdomain_codeset... (cached) yes
checking for msgfmt... (cached) /usr/bin/msgfmt
checking for dcgettext... (cached) yes
checking if msgfmt accepts -c... yes
checking for gmsgfmt... (cached) /usr/bin/msgfmt
checking for xgettext... (cached) /usr/bin/xgettext
checking for catalogs to be installed...  af am ang ar as az az_IR be be@latin bg bn bn_IN br bs ca ca@valencia cs cy da de dz el en_CA en_GB eo es et eu fa fi fr ga gl gu he hi hr hu hy ia id io is it ja ka kn ko ku li lt lv mai mi mk ml mn mr ms nb ne nl nn nso oc or pa pl ps pt pt_BR ro ru rw si sk sl sq sr sr@latin sr@ije sv ta te th tk tr tt uk ur uz uz@cyrillic vi wa xh yi zh_CN zh_HK zh_TW
checking for extra flags to get ANSI library prototypes... none needed
checking for the BeOS... no
checking for HP-UX... no
checking for extra flags for POSIX compliance... none needed
checking for arm-linux-pkg-config... (cached) /opt/freescale/ltib/usr/bin/pkg-config
checking pkg-config is at least version 0.16... yes
checking for GLIB - version >= 2.17.6... cross compiling; assumed OK...
yes (version 2.18.1)
checking for bind_textdomain_codeset... (cached) yes
checking for pwd.h... (cached) yes
checking for sys/time.h... (cached) yes
checking for unistd.h... (cached) yes
checking for ftw.h... (cached) yes
checking for GNU ftw extensions... yes
checking for ANSI C header files... (cached) yes
checking for an ANSI C-conforming const... (cached) yes
checking return type of signal handlers... (cached) void
checking for stdlib.h... (cached) yes
checking for unistd.h... (cached) yes
checking for getpagesize... (cached) yes
checking for working mmap... (cached) no
checking for mallinfo... (cached) yes
checking for getresuid... (cached) yes
checking for uid_t in sys/types.h... (cached) yes
checking for fd_set... yes, found in sys/types.h
checking for wchar.h... yes
checking for wctype.h... yes
checking for iswalnum... (cached) yes
checking if iswalnum() and friends are properly defined... yes
checking for uxtheme.h... no
checking for crt_externs.h... (cached) no
checking for _NSGetEnviron... (cached) no
checking whether to build gmodulized gdk-pixbuf... yes
checking whether dynamic modules work... yes
checking for TIFFReadRGBAImageOriented in -ltiff... (cached) yes
checking for tiffio.h... (cached) yes
checking for jpeg_destroy_decompress in -ljpeg... (cached) yes
checking for jpeglib.h... yes
checking for jpeg_simple_progression in -ljpeg... (cached) yes
checking for libpng12... yes
checking pixbuf loaders to build...
checking immodules to build...
checking for sys/wait.h that is POSIX.1 compatible... (cached) yes
checking return type of signal handlers... (cached) void
checking for sys/systeminfo.h... (cached) no
checking for sys/sysinfo.h... (cached) yes
checking for mediaLib 2.3... checking for mlib_ImageSetStruct in -lmlib... (cached) no
checking for x86 platform... no
checking for gdk-pixbuf-csource... (cached) /usr/bin/gdk-pixbuf-csource
checking for gtk-update-icon-cache... (cached) /usr/bin/gtk-update-icon-cache
checking for X... (cached) libraries /usr/lib, headers /usr/include
checking whether -R must be followed by a space... neither works
checking for dnet_ntoa in -ldnet... (cached) no
checking for dnet_ntoa in -ldnet_stub... (cached) no
checking for gethostbyname... (cached) yes
checking for connect... (cached) yes
checking for remove... (cached) yes
checking for shmat... (cached) yes
checking for IceConnectionNumber in -lICE... (cached) no
checking for XOpenDisplay... (cached) yes
checking for XextFindDisplay... (cached) yes
checking for XRenderQueryExtension... (cached) yes
checking if <X11/extensions/XIproto.h> is needed for xReply... no
checking for XConvertCase... (cached) yes
checking for XInternAtoms... (cached) yes
checking for XAddConnectionWatch... (cached) yes
checking for XkbQueryExtension... (cached) yes
checking for XShapeCombineMask... (cached) yes
checking for XSyncQueryExtension... (cached) yes
checking for X11/extensions/sync.h... (cached) yes
checking for XShmAttach... (cached) yes
checking for sys/ipc.h... (cached) yes
checking for sys/shm.h... (cached) yes
checking X11/extensions/XShm.h... yes
checking for Xinerama support on XFree86... checking for XineramaQueryExtension in -lXinerama... (cached) no
no
checking Pango flags... -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1   -L/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib -lpangocairo-1.0 -lpango-1.0 -lcairo -lgobject-2.0 -lgmodule-2.0 -lglib-2.0 
checking ATK flags... -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/atk-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include   -L/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib -latk-1.0 -lgobject-2.0 -lgmodule-2.0 -lglib-2.0 
checking for library containing gethostent... (cached) none required
checking for library containing setsockopt... (cached) none required
checking for library containing connect... (cached) none required
checking for struct sockaddr_un.sun_len... (cached) no
checking for cairo-pdf.h... (cached) yes
checking for cairo-ps.h... (cached) yes
checking whether to build gtk-doc documentation... no
checking for gtkdoc-check... no
checking for db2html... (cached) false
configure: creating ./config.status
config.status: creating config.h.win32
config.status: creating gtk-zip.sh
config.status: creating Makefile
config.status: creating gdk-pixbuf-2.0.pc
config.status: creating gdk-2.0.pc
config.status: creating gtk+-2.0.pc
config.status: creating gtk+-unix-print-2.0.pc
config.status: creating gail.pc
config.status: creating gdk-pixbuf-2.0-uninstalled.pc
config.status: creating gdk-2.0-uninstalled.pc
config.status: creating gtk+-2.0-uninstalled.pc
config.status: creating gail-uninstalled.pc
config.status: creating m4macros/Makefile
config.status: creating po/Makefile.in
config.status: WARNING:  'po/Makefile.in.in' seems to ignore the --datarootdir setting
config.status: creating po-properties/Makefile.in
config.status: WARNING:  'po-properties/Makefile.in.in' seems to ignore the --datarootdir setting
config.status: creating demos/Makefile
config.status: creating demos/gtk-demo/Makefile
config.status: creating demos/gtk-demo/geninclude.pl
config.status: creating tests/Makefile
config.status: creating docs/Makefile
config.status: creating docs/reference/Makefile
config.status: creating docs/reference/gdk-pixbuf/Makefile
config.status: creating docs/reference/gdk-pixbuf/version.xml
config.status: creating docs/reference/gdk/Makefile
config.status: creating docs/reference/gdk/version.xml
config.status: creating docs/reference/gtk/Makefile
config.status: creating docs/reference/gtk/version.xml
config.status: creating docs/reference/libgail-util/Makefile
config.status: creating docs/faq/Makefile
config.status: creating docs/tools/Makefile
config.status: creating docs/tutorial/Makefile
config.status: creating gdk-pixbuf/Makefile
config.status: creating gdk-pixbuf/gdk_pixbuf.rc
config.status: creating gdk-pixbuf/gdk-pixbuf-features.h
config.status: creating gdk-pixbuf/pixops/Makefile
config.status: creating gdk/Makefile
config.status: creating gdk/x11/Makefile
config.status: creating gdk/win32/Makefile
config.status: creating gdk/win32/rc/Makefile
config.status: creating gdk/win32/rc/gdk.rc
config.status: creating gdk/quartz/Makefile
config.status: creating gdk/directfb/Makefile
config.status: creating gdk/tests/Makefile
config.status: creating gtk/Makefile
config.status: creating gtk/makefile.msc
config.status: creating gtk/gtkversion.h
config.status: creating gtk/gtk-win32.rc
config.status: creating gtk/theme-bits/Makefile
config.status: creating gtk/tests/Makefile
config.status: creating modules/Makefile
config.status: creating modules/other/Makefile
config.status: creating modules/other/gail/Makefile
config.status: creating modules/other/gail/libgail-util/Makefile
config.status: creating modules/other/gail/tests/Makefile
config.status: creating modules/engines/Makefile
config.status: creating modules/engines/pixbuf/Makefile
config.status: creating modules/engines/ms-windows/Makefile
config.status: creating modules/engines/ms-windows/Theme/Makefile
config.status: creating modules/engines/ms-windows/Theme/gtk-2.0/Makefile
config.status: creating modules/input/Makefile
config.status: creating modules/printbackends/Makefile
config.status: creating modules/printbackends/cups/Makefile
config.status: creating modules/printbackends/lpr/Makefile
config.status: creating modules/printbackends/file/Makefile
config.status: creating modules/printbackends/test/Makefile
config.status: creating perf/Makefile
config.status: creating contrib/Makefile
config.status: creating contrib/gdk-pixbuf-xlib/Makefile
config.status: creating contrib/gdk-pixbuf-xlib/gdk-pixbuf-xlib-2.0.pc
config.status: creating config.h
config.status: config.h is unchanged
config.status: executing depfiles commands
config.status: executing default-1 commands
config.status: executing default-2 commands
config.status: executing gdk/gdkconfig.h commands
config.status: gdk/gdkconfig.h is unchanged
configuration:
        target: x11
+ perl -pi -e s,^sys_lib_search_path_spec=.*,sys_lib_search_path_spec=, libtool
+ make
make  all-recursive
make[1]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3'
Making all in po
make[2]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/po'
make[2]: Nothing to be done for `all'.
make[2]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/po'
Making all in po-properties
make[2]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/po-properties'
make[2]: Nothing to be done for `all'.
make[2]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/po-properties'
Making all in gdk-pixbuf
make[2]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk-pixbuf'
make[2]: Warning: File `.deps/test-gdk-pixbuf.Po' has modification time 8.3e+02 s in the future
make  all-recursive
make[3]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk-pixbuf'
make[3]: Warning: File `.deps/test-gdk-pixbuf.Po' has modification time 8.3e+02 s in the future
Making all in pixops
make[4]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk-pixbuf/pixops'
make[4]: Nothing to be done for `all'.
make[4]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk-pixbuf/pixops'
make[4]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk-pixbuf'
make[4]: Warning: File `.deps/test-gdk-pixbuf.Po' has modification time 8.3e+02 s in the future
make[4]: warning:  Clock skew detected.  Your build may be incomplete.
make[4]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk-pixbuf'
make[3]: warning:  Clock skew detected.  Your build may be incomplete.
make[3]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk-pixbuf'
make[2]: warning:  Clock skew detected.  Your build may be incomplete.
make[2]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk-pixbuf'
Making all in gdk
make[2]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk'
make[2]: Warning: File `stamp-gc-h' has modification time 8.4e+02 s in the future
make  all-recursive
make[3]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk'
Making all in x11
make[4]: Entering directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk/x11'
make[4]: Warning: File `.deps/gdkinput.Plo' has modification time 8.4e+02 s in the future
if /bin/bash ../../libtool --mode=compile gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1      -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES  -I/usr/include  -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkapplaunchcontext-x11.lo -MD -MP -MF ".deps/gdkapplaunchcontext-x11.Tpo" \
      -c -o gdkapplaunchcontext-x11.lo `test -f 'gdkapplaunchcontext-x11.c' || echo './'`gdkapplaunchcontext-x11.c; \
    then mv -f ".deps/gdkapplaunchcontext-x11.Tpo" ".deps/gdkapplaunchcontext-x11.Plo"; \
    else rm -f ".deps/gdkapplaunchcontext-x11.Tpo"; exit 1; \
    fi
if /bin/bash ../../libtool --mode=compile gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1      -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES  -I/usr/include  -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkasync.lo -MD -MP -MF ".deps/gdkasync.Tpo" \
      -c -o gdkasync.lo `test -f 'gdkasync.c' || echo './'`gdkasync.c; \
    then mv -f ".deps/gdkasync.Tpo" ".deps/gdkasync.Plo"; \
    else rm -f ".deps/gdkasync.Tpo"; exit 1; \
    fi
if /bin/bash ../../libtool --mode=compile gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1      -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES  -I/usr/include  -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkcolor-x11.lo -MD -MP -MF ".deps/gdkcolor-x11.Tpo" \
      -c -o gdkcolor-x11.lo `test -f 'gdkcolor-x11.c' || echo './'`gdkcolor-x11.c; \
    then mv -f ".deps/gdkcolor-x11.Tpo" ".deps/gdkcolor-x11.Plo"; \
    else rm -f ".deps/gdkcolor-x11.Tpo"; exit 1; \
    fi
if /bin/bash ../../libtool --mode=compile gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1      -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES  -I/usr/include  -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkcursor-x11.lo -MD -MP -MF ".deps/gdkcursor-x11.Tpo" \
      -c -o gdkcursor-x11.lo `test -f 'gdkcursor-x11.c' || echo './'`gdkcursor-x11.c; \
    then mv -f ".deps/gdkcursor-x11.Tpo" ".deps/gdkcursor-x11.Plo"; \
    else rm -f ".deps/gdkcursor-x11.Tpo"; exit 1; \
    fi
if /bin/bash ../../libtool --mode=compile gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1      -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES  -I/usr/include  -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkdisplay-x11.lo -MD -MP -MF ".deps/gdkdisplay-x11.Tpo" \
      -c -o gdkdisplay-x11.lo `test -f 'gdkdisplay-x11.c' || echo './'`gdkdisplay-x11.c; \
    then mv -f ".deps/gdkdisplay-x11.Tpo" ".deps/gdkdisplay-x11.Plo"; \
    else rm -f ".deps/gdkdisplay-x11.Tpo"; exit 1; \
    fi
if /bin/bash ../../libtool --mode=compile gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1      -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES  -I/usr/include  -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkdnd-x11.lo -MD -MP -MF ".deps/gdkdnd-x11.Tpo" \
      -c -o gdkdnd-x11.lo `test -f 'gdkdnd-x11.c' || echo './'`gdkdnd-x11.c; \
    then mv -f ".deps/gdkdnd-x11.Tpo" ".deps/gdkdnd-x11.Plo"; \
    else rm -f ".deps/gdkdnd-x11.Tpo"; exit 1; \
    fi
if /bin/bash ../../libtool --mode=compile gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1      -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES  -I/usr/include  -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkdrawable-x11.lo -MD -MP -MF ".deps/gdkdrawable-x11.Tpo" \
      -c -o gdkdrawable-x11.lo `test -f 'gdkdrawable-x11.c' || echo './'`gdkdrawable-x11.c; \
    then mv -f ".deps/gdkdrawable-x11.Tpo" ".deps/gdkdrawable-x11.Plo"; \
    else rm -f ".deps/gdkdrawable-x11.Tpo"; exit 1; \
    fi
if /bin/bash ../../libtool --mode=compile gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1      -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES  -I/usr/include  -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkevents-x11.lo -MD -MP -MF ".deps/gdkevents-x11.Tpo" \
      -c -o gdkevents-x11.lo `test -f 'gdkevents-x11.c' || echo './'`gdkevents-x11.c; \
    then mv -f ".deps/gdkevents-x11.Tpo" ".deps/gdkevents-x11.Plo"; \
    else rm -f ".deps/gdkevents-x11.Tpo"; exit 1; \
    fi
 gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1 -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES -I/usr/include -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkasync.lo -MD -MP -MF .deps/gdkasync.Tpo -c gdkasync.c  -fPIC -DPIC -o .libs/gdkasync.o
 gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1 -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES -I/usr/include -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkapplaunchcontext-x11.lo -MD -MP -MF .deps/gdkapplaunchcontext-x11.Tpo -c gdkapplaunchcontext-x11.c  -fPIC -DPIC -o .libs/gdkapplaunchcontext-x11.o
 gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1 -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES -I/usr/include -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkcursor-x11.lo -MD -MP -MF .deps/gdkcursor-x11.Tpo -c gdkcursor-x11.c  -fPIC -DPIC -o .libs/gdkcursor-x11.o
 gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1 -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES -I/usr/include -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkdrawable-x11.lo -MD -MP -MF .deps/gdkdrawable-x11.Tpo -c gdkdrawable-x11.c  -fPIC -DPIC -o .libs/gdkdrawable-x11.o
 gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1 -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES -I/usr/include -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkcolor-x11.lo -MD -MP -MF .deps/gdkcolor-x11.Tpo -c gdkcolor-x11.c  -fPIC -DPIC -o .libs/gdkcolor-x11.o
 gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1 -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES -I/usr/include -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkdnd-x11.lo -MD -MP -MF .deps/gdkdnd-x11.Tpo -c gdkdnd-x11.c  -fPIC -DPIC -o .libs/gdkdnd-x11.o
 gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1 -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES -I/usr/include -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkdisplay-x11.lo -MD -MP -MF .deps/gdkdisplay-x11.Tpo -c gdkdisplay-x11.c  -fPIC -DPIC -o .libs/gdkdisplay-x11.o
 gcc -DHAVE_CONFIG_H -I. -I. -I../.. -DG_LOG_DOMAIN=\"Gdk\" -DGDK_COMPILATION -I../.. -I../../gdk -I../../gdk -DG_DISABLE_CAST_CHECKS -pthread -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/glib-2.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/lib/glib-2.0/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pango-1.0 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/cairo -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/freetype2 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/libpng12 -I/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rootfs/usr/include/pixman-1 -DG_DISABLE_SINGLE_INCLUDES -DATK_DISABLE_SINGLE_INCLUDES -DGDK_PIXBUF_DISABLE_SINGLE_INCLUDES -DGTK_DISABLE_SINGLE_INCLUDES -I/usr/include -DGDK_PIXBUF_DISABLE_DEPRECATED -g -O2 -Wall -MT gdkevents-x11.lo -MD -MP -MF .deps/gdkevents-x11.Tpo -c gdkevents-x11.c  -fPIC -DPIC -o .libs/gdkevents-x11.o
gdkdrawable-x11.c:32:24: error: cairo-xlib.h: No such file or directory
gdkdrawable-x11.c: In function '_gdk_x11_drawable_update_size':
gdkdrawable-x11.c:238: warning: implicit declaration of function 'cairo_xlib_surface_set_size'
gdkdrawable-x11.c: In function 'gdk_x11_ref_cairo_surface':
gdkdrawable-x11.c:1469: warning: implicit declaration of function 'cairo_xlib_surface_create'
gdkdrawable-x11.c:1472: warning: assignment makes pointer from integer without a cast
gdkdrawable-x11.c:1474: warning: implicit declaration of function 'cairo_xlib_surface_create_for_bitmap'
gdkdrawable-x11.c:1477: warning: assignment makes pointer from integer without a cast
make[4]: *** [gdkdrawable-x11.lo] Error 1
make[4]: *** Waiting for unfinished jobs....
gdkcursor-x11.c: In function 'IA__gdk_cursor_new_from_pixbuf':
gdkcursor-x11.c:816: warning: pointer targets in passing argument 2 of 'IA__gdk_bitmap_create_from_data' differ in signedness
gdkcursor-x11.c:819: warning: pointer targets in passing argument 2 of 'IA__gdk_bitmap_create_from_data' differ in signedness
gdkevents-x11.c: In function 'IA__gdk_x11_screen_get_window_manager_name':
gdkevents-x11.c:2721: warning: dereferencing type-punned pointer will break strict-aliasing rules
gdkevents-x11.c: In function 'IA__gdk_x11_screen_supports_net_wm_hint':
gdkevents-x11.c:2821: warning: dereferencing type-punned pointer will break strict-aliasing rules
make[4]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk/x11'
make[3]: *** [all-recursive] Error 1
make[3]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk'
make[2]: *** [all] Error 2
make[2]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3/gdk'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/rpm/BUILD/gtk+-2.14.3'
make: *** [all] Error 2
error: Bad exit status from /home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/tmp/rpm-tmp.95024 (%build)


RPM build errors:
    Bad exit status from /home/satyam/IMX35_Linux31/L2.6.31_09.12.01_SDK_source/imx28_2_Sep/ltib/tmp/rpm-tmp.95024 (%build)
Build time for gtk2: 24 seconds

Failed building gtk2


f_buildrpms() returned an error, exiting
traceback:
 main:560


Started: Tue Sep  6 16:06:41 2011
Ended:   Tue Sep  6 16:12:43 2011
Elapsed: 362 seconds

These packages failed to build:
gtk2

Build Failed

Exiting on error or interrupt

タグ(1)
0 件の賞賛
返信
0 返答(返信)