IMX 25 WinCE 6.0 Bootloader for NAND flash.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 25 WinCE 6.0 Bootloader for NAND flash.

2,794 Views
aswinpp
Contributor I

Hi All,

     I am a newbie on imx platform and unfortunately i lost the preloaded WinCE 6.0 Bootloader in NAND flash.

So I can't boot the device.

I tried to program Eboot.nb0 and XLDR.nb0 to NAND as well as SD Card using ATK, B@@ut its not loading Bootloaders.

Can anybody give me the correct procedure to program bootloader to NAND and SD Card.. Also provide Working Bootloader binaries for WinCE6.0 IMX25 platform.

Thanks and Regards

Aswin

Labels (2)
0 Kudos
Reply
1 Reply

2,149 Views
igorpadykov
NXP Employee
NXP Employee

Hi ASWIN

please look below

IMX25_WINCE600_DEMOFILES_09_12  : 2009.12 Windows Embedded CE 6.0 Demo Images.

IMX25_PDK09_12_WIN60DOCS_BUNDLE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply