IM8Plus ETH0 slow ping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IM8Plus ETH0 slow ping

1,381 Views
ilanganor1
Contributor III
we are using IMX8PLUS NXP EVB
 
when connecting eth0 and eth1 to PC we need to get ping <0.5msec
 
on eth1, great results, we doget 0.3msec
on eth0 the result is , ~0.8 msec
 
 
please also see this: link
 
 
how can I improve latency? 
 
maybe setting the eth to disable sleep when not used? (no power limitations in this implementation)

please advice
0 Kudos
Reply
2 Replies

1,345 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @ilanganor1 

Reply from SE team:

ENET1 port and ENET_QoS port are different IPs,

when transmitting same length of frames, the rate may be different.

Suggest customer set frame length to MTU(1500bytes) for test.

we ever compared these two ports using test-center, when sending MTU packets(1500bytes),  

ENET1 port and ENET_QoS port can both reach the line-rate.

 

Best Regards

Zhiming

0 Kudos
Reply

1,329 Views
ilanganor1
Contributor III

ok, so maybe I need to check diffrentlly

 

I want to make sure packet latency <1msec for both eth0 and eth1, can you instruct a recommanded setup for that? 

0 Kudos
Reply