IM8MQ using ECSPI with DMA in M4 Core.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IM8MQ using ECSPI with DMA in M4 Core.

3,046 Views
siva3
Contributor I

Hi,

I was wondering if there is any example or tutorial to show how to use DMA in M4 core.

I need to transfer 16-bit data of length 16,000 in full duplex (send and receive simultaneously) at 32MHz, for this I think the normal transfer function won't work. So I was wondering if I could use DMA but in ECSPI driver I could only find DMA Init function and also I couldn't find any driver for DMA.

Is there any documentation relating to this ??

0 Kudos
Reply
3 Replies

2,926 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sivaram

some examples can be found in SDK_2.6.0_EVK-MIMX8MM (I am not aware of

examples for i.MX8MQ), SDK can be obtained from https://mcuxpresso.nxp.com/en/select 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,926 Views
siva3
Contributor I

Hi Igor,

The driver for SDMA seems to be missing in IMX8MQ :smileysad:..Can we expect support for SDMA on IMX8MQ  anytime soon..?

Thanks and Regards,

Sivaram SR

0 Kudos
Reply

2,926 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sivaram

I do not think so.

Best regards
igor

0 Kudos
Reply