IM.X35 no serial(console) input (3.11.1)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IM.X35 no serial(console) input (3.11.1)

跳至解决方案
1,624 次查看
maxvankessel
Contributor II

I'm using an I.MX35 SOC with the freescale linux mainline  (3.11.1).

I'm unable to receive any bytes from the serial input, the serial input/output (UART3) is connected to the console.

Someone an idea what is wrong?

标签 (1)
0 项奖励
回复
1 解答
1,555 次查看
maxvankessel
Contributor II

Thanks,

Both Tx and Rx were configured for different pins.

Transmit was working (not configured), but receiver wasn't doing a thing.

Fixed the problem by changing the pins to the correct RS232 pins.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,556 次查看
maxvankessel
Contributor II

Thanks,

Both Tx and Rx were configured for different pins.

Transmit was working (not configured), but receiver wasn't doing a thing.

Fixed the problem by changing the pins to the correct RS232 pins.

0 项奖励
回复
1,555 次查看
fabio_estevam
NXP Employee
NXP Employee

Does U-boot work? It would help if you could post your board file, boot logs, etc.

0 项奖励
回复
1,554 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Max,

I recommend you first to check the serial configurations, the speed is 115200 for example. And make sure if your board is working.

Best Regards

Dan

0 项奖励
回复