IEEE1588 on i.mx7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEEE1588 on i.mx7

1,453 Views
ryanschroeder
NXP Employee
NXP Employee


Do any of the i.mx7 variants have IEEE 1588 built into the dual GigE ports?

Labels (2)
0 Kudos
Reply
1 Reply

1,311 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ryan

please check p.1467 i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

it shows ENET1,2 1588 signals and Chanpter 11.1 Ethernet MAC (ENET)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply