I2S interface for iMX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2S interface for iMX6Solo

1,659 Views
jasonteoh
Contributor I

Hi Sir/Mdm,

Currently I'm using the I.MX6Solo and wanted to integrate with NXP Dirana 3 using I2S. Below NXP FAE had some concern.

NXP FAE concern: You might need to check with iMX6 about their I2S interface pad, as you know NXP Dirana 3 I2S is configured in current mode which will help to prevent the interference to the radio performance. A conversion might need to require to have the matching mode e.g. from CMOS to Current and vice versus.

Can you help me check the I2S interface for iMX6 is current or under CMOS?

Regard's

Jason.

Tags (1)
0 Kudos
Reply
1 Reply

1,392 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jason

iMX6 I2S interface is CMOS, specs are given in

IMX6DQCEC Table 22. GPIO I/O DC Parameters

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply