I2S interface for iMX6Solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2S interface for iMX6Solo

1,650件の閲覧回数
jasonteoh
Contributor I

Hi Sir/Mdm,

Currently I'm using the I.MX6Solo and wanted to integrate with NXP Dirana 3 using I2S. Below NXP FAE had some concern.

NXP FAE concern: You might need to check with iMX6 about their I2S interface pad, as you know NXP Dirana 3 I2S is configured in current mode which will help to prevent the interference to the radio performance. A conversion might need to require to have the matching mode e.g. from CMOS to Current and vice versus.

Can you help me check the I2S interface for iMX6 is current or under CMOS?

Regard's

Jason.

タグ(1)
0 件の賞賛
返信
1 返信

1,383件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jason

iMX6 I2S interface is CMOS, specs are given in

IMX6DQCEC Table 22. GPIO I/O DC Parameters

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信