I2C3 from EPDC Group

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C3 from EPDC Group

1,366 Views
pankajrana
Contributor III

Hi,

In the current design we are interfacing a 8 inch EPD, 16 data lines with MCIMX6SLEVK - i.Mx6 SoloLite EVK. The signals "EPDC_SDCE3" and "EPDC_SDCE2" are currently not used. So when we enable the EPDC , is it possible to use these two signals for I2C3 in ALT1 mode ?

--Pankaj Rana

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,212 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

yes if not used for EPDC, these pins can be used for other purposes for example

as I2C3 in ALT1 mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply